<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K342 SPI interrupt not triggered in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1651482#M22976</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210668"&gt;@bbaskii&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Just to be sure, did you enable the SPI interrupt?&lt;/P&gt;
&lt;P&gt;If you did it, could you verify if the interrupt is correctly addressed?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
    <pubDate>Tue, 16 May 2023 20:41:59 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2023-05-16T20:41:59Z</dc:date>
    <item>
      <title>S32K342 SPI interrupt not triggered</title>
      <link>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1649325#M22864</link>
      <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;I am working on SPI communication with PMIC. SPI interrupts are not triggered when it is not receiving any data or when TX buffer is empty. If anyone faced similar situation and overcome please share the solution to fix the issue.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;bbaskii&lt;/P&gt;</description>
      <pubDate>Fri, 12 May 2023 10:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1649325#M22864</guid>
      <dc:creator>bbaskii</dc:creator>
      <dc:date>2023-05-12T10:17:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32K342 SPI interrupt not triggered</title>
      <link>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1651482#M22976</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210668"&gt;@bbaskii&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Just to be sure, did you enable the SPI interrupt?&lt;/P&gt;
&lt;P&gt;If you did it, could you verify if the interrupt is correctly addressed?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 20:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1651482#M22976</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-05-16T20:41:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K342 SPI interrupt not triggered</title>
      <link>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1652024#M23008</link>
      <description>&lt;P&gt;Hi VaneB,&lt;/P&gt;&lt;P&gt;Thanks for the reply. My project uses the EBTresos and Autosar OS. I have enabled the interrupt in the EBTresOS inside&lt;/P&gt;&lt;P&gt;Platform-&amp;gt;Interrupt Controller and added&amp;nbsp;Lpspi_Ip_LPSPI_2_IRQHandler in Generic Interrupt Settings Tab. I got the below linker error.&lt;/P&gt;&lt;P&gt;Linking main.elf&lt;BR /&gt;[elxr] (error #412) unresolved symbols: 2&lt;BR /&gt;LPUART_UART_IP_0_IRQHandler from IntCtrl_Ip_Cfg.o&lt;BR /&gt;Lpspi_Ip_LPSPI_2_IRQHandler from IntCtrl_Ip_Cfg.o&lt;/P&gt;&lt;P&gt;[elxr] (error) errors during processing&lt;BR /&gt;make: *** [makefile:266: main.elf] Error 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this information helps to look further. Please help me to fix the issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks In Advance,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;bbaskii&lt;/P&gt;</description>
      <pubDate>Wed, 17 May 2023 11:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1652024#M23008</guid>
      <dc:creator>bbaskii</dc:creator>
      <dc:date>2023-05-17T11:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K342 SPI interrupt not triggered</title>
      <link>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1654061#M23094</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210668"&gt;@bbaskii&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you provide me with more details about how are you configuring the interruptions?&lt;/P&gt;</description>
      <pubDate>Fri, 19 May 2023 22:28:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1654061#M23094</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-05-19T22:28:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K342 SPI interrupt not triggered</title>
      <link>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1658105#M23322</link>
      <description>&lt;P&gt;Hi VaneB,&lt;/P&gt;&lt;P&gt;Thanks for the reply. I got the linker error after i have enabled the interrupt in EBTresos configuration tool-&amp;gt;Platform tab. Please refer it to&amp;nbsp;EBTresos_Platform_Interrupt4.jpg. I have added interrupt configuration and enabled while i have tested. I have given below screenshot to show the method i have followed for enabling the interrupt. But i followed those steps i got the interrupt. Hope this help to analyze further.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;bbaskii&lt;/P&gt;</description>
      <pubDate>Fri, 26 May 2023 05:54:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1658105#M23322</guid>
      <dc:creator>bbaskii</dc:creator>
      <dc:date>2023-05-26T05:54:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K342 SPI interrupt not triggered</title>
      <link>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1659298#M23372</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210668"&gt;@bbaskii&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Normally, It is needed to enable the flag "USING_OS_AUTOSAROS" inside the Base driver. One additional point is how you are defining it inside the Autosar OS.&lt;/P&gt;
&lt;P&gt;For example:&lt;/P&gt;
&lt;P&gt;ISR name: MCL_FLEXIO_ISR&lt;/P&gt;
&lt;P&gt;sys_disableIsrSource(139);&lt;/P&gt;
&lt;P&gt;sys_enableIsrSource(139, 7);&lt;/P&gt;
&lt;P&gt;sys_registerIsrHandler(139, MCL_FLEXIO_ISR);&lt;/P&gt;
&lt;P&gt;where:&lt;/P&gt;
&lt;P&gt;139: NVIC Interrupt ID of FLEXIO module&lt;BR /&gt;7: The priority&lt;/P&gt;</description>
      <pubDate>Mon, 29 May 2023 20:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1659298#M23372</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-05-29T20:50:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32K342 SPI interrupt not triggered</title>
      <link>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1662693#M23563</link>
      <description>Hi VaneB,&lt;BR /&gt;When i enable USING_OS_AUTOSAROS in EBTresos, got multiple error in the tool. We are using EBTresos version 29. But without that we configured the interrupt in ETAS OS and verified few interrupts which are working. Thanks for your support.</description>
      <pubDate>Fri, 02 Jun 2023 13:32:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K342-SPI-interrupt-not-triggered/m-p/1662693#M23563</guid>
      <dc:creator>bbaskii</dc:creator>
      <dc:date>2023-06-02T13:32:37Z</dc:date>
    </item>
  </channel>
</rss>