<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: code hangs on WDOG_EWM_IRQHandler()</title>
    <link>https://community.nxp.com/t5/S32K/code-hangs-on-WDOG-EWM-IRQHandler/m-p/1651099#M22963</link>
    <description>&lt;P&gt;Hi, There is no other ISR used other than UART1 and 2. But this problem was persistent. After lots of effords we decided to create new workspace and it worked in new WS.&lt;/P&gt;&lt;P&gt;this is kinda illogical situation because code was not edited. same code with same stack size worked after importing in new workspace.&lt;/P&gt;</description>
    <pubDate>Tue, 16 May 2023 11:00:44 GMT</pubDate>
    <dc:creator>s32k146_ige</dc:creator>
    <dc:date>2023-05-16T11:00:44Z</dc:date>
    <item>
      <title>code hangs on WDOG_EWM_IRQHandler()</title>
      <link>https://community.nxp.com/t5/S32K/code-hangs-on-WDOG-EWM-IRQHandler/m-p/1650175#M22916</link>
      <description>&lt;P&gt;My code has started to hang in&amp;nbsp;WDOG_EWM_IRQHandler (), it was working while ago. there is apparent no reason to have this behavior.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have 2 freertos task running, if i disable task 2, it runs fine and doesnt hang in default ISR. But if i enable task 2 it hangs, in task 2 i have added 10ms delay at very start. and while single stepping this vTaskdelay sends the code in default ISR&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;static void task2()
{
	uint32_t lu32Counter = 0;
	// wait 10ms
	vTaskDelay(pdMS_TO_TICKS(10));&lt;/LI-CODE&gt;&lt;P&gt;I have 2 interrupt running 1 for uart1 and 1 for uart2. apart from that i wanted to use GPIO interrupt but it is disabled now.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also added following code to disable WDOG, at start&lt;/P&gt;&lt;P&gt;I have also tried increasing the TASK stack depth and had no effect&lt;/P&gt;&lt;LI-CODE lang="c"&gt;  WDOG-&amp;gt;CNT=0xD928C520;     /* Unlock watchdog 		*/
  WDOG-&amp;gt;TOVAL=0x0000FFFF;   /* Maximum timeout value 	*/
  WDOG-&amp;gt;CS = 0x00002100;    /* Disable watchdog 		*/&lt;/LI-CODE&gt;&lt;P&gt;can anyone guide me in diagnosing this fault ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 09:03:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/code-hangs-on-WDOG-EWM-IRQHandler/m-p/1650175#M22916</guid>
      <dc:creator>s32k146_ige</dc:creator>
      <dc:date>2023-05-15T09:03:22Z</dc:date>
    </item>
    <item>
      <title>Re: code hangs on WDOG_EWM_IRQHandler()</title>
      <link>https://community.nxp.com/t5/S32K/code-hangs-on-WDOG-EWM-IRQHandler/m-p/1650949#M22954</link>
      <description>&lt;P&gt;Hi Sushant Naik,&lt;/P&gt;
&lt;P&gt;The Default_ISR is probably a fault exception, I assume you don't have HardFault_Handler() implemented in the project.&lt;/P&gt;
&lt;P&gt;Can you confirm it by reading the CFSR core register in the Default_ISR and debug it?&lt;/P&gt;
&lt;P&gt;You should be able to find the type of the exception and the PC address of the fault instruction.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 08:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/code-hangs-on-WDOG-EWM-IRQHandler/m-p/1650949#M22954</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-05-16T08:26:44Z</dc:date>
    </item>
    <item>
      <title>Re: code hangs on WDOG_EWM_IRQHandler()</title>
      <link>https://community.nxp.com/t5/S32K/code-hangs-on-WDOG-EWM-IRQHandler/m-p/1651099#M22963</link>
      <description>&lt;P&gt;Hi, There is no other ISR used other than UART1 and 2. But this problem was persistent. After lots of effords we decided to create new workspace and it worked in new WS.&lt;/P&gt;&lt;P&gt;this is kinda illogical situation because code was not edited. same code with same stack size worked after importing in new workspace.&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 11:00:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/code-hangs-on-WDOG-EWM-IRQHandler/m-p/1651099#M22963</guid>
      <dc:creator>s32k146_ige</dc:creator>
      <dc:date>2023-05-16T11:00:44Z</dc:date>
    </item>
  </channel>
</rss>