<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SACKERR causing reset during STOP2 entry with CAN pretended network in S32K</title>
    <link>https://community.nxp.com/t5/S32K/SACKERR-causing-reset-during-STOP2-entry-with-CAN-pretended/m-p/1650848#M22952</link>
    <description>&lt;P&gt;Even after configuring pretended network, while entering STOP2 mode CAN bus didn't go into IDLE state. De-initializing and re-initializing CAN before configuring pretended network fixed this.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 16 May 2023 06:41:48 GMT</pubDate>
    <dc:creator>dinesh_balaji</dc:creator>
    <dc:date>2023-05-16T06:41:48Z</dc:date>
    <item>
      <title>SACKERR causing reset during STOP2 entry with CAN pretended network</title>
      <link>https://community.nxp.com/t5/S32K/SACKERR-causing-reset-during-STOP2-entry-with-CAN-pretended/m-p/1646122#M22694</link>
      <description>&lt;P&gt;I'm trying to put the MCU(S32K146) into STOP2 mode with CAN wake up. I'm using pretended network feature on CAN0.&lt;BR /&gt;I'm disabling all other peripherals except CAN0 before entering STOP2 power mode. But, the MCU resets after entering STOP2 mode with reset cause as SACKERR(stop acknowledge error).&amp;nbsp;&lt;BR /&gt;If I try entering STOP2 mode with CAN0 disabled, I'm not seeing any reset.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I'm on RUN power mode before STOP2 entry and I followed the steps mentioned in the application note AN5425.&lt;/P&gt;&lt;P&gt;Also, Is there any way to identify which peripheral failed to acknowledge stop mode entry and caused the SACKERR reset?&lt;/P&gt;</description>
      <pubDate>Mon, 08 May 2023 06:10:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SACKERR-causing-reset-during-STOP2-entry-with-CAN-pretended/m-p/1646122#M22694</guid>
      <dc:creator>dinesh_balaji</dc:creator>
      <dc:date>2023-05-08T06:10:30Z</dc:date>
    </item>
    <item>
      <title>Re: SACKERR causing reset during STOP2 entry with CAN pretended network</title>
      <link>https://community.nxp.com/t5/S32K/SACKERR-causing-reset-during-STOP2-entry-with-CAN-pretended/m-p/1646232#M22701</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to the&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-Pretended-Networking-STOP-mode-test/ta-p/1101224" target="_self"&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;Example S32K144 FlexCAN Pretended Networking STOP mode test S32DS.ARM.2.2&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 08 May 2023 07:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SACKERR-causing-reset-during-STOP2-entry-with-CAN-pretended/m-p/1646232#M22701</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-05-08T07:52:58Z</dc:date>
    </item>
    <item>
      <title>Re: SACKERR causing reset during STOP2 entry with CAN pretended network</title>
      <link>https://community.nxp.com/t5/S32K/SACKERR-causing-reset-during-STOP2-entry-with-CAN-pretended/m-p/1650848#M22952</link>
      <description>&lt;P&gt;Even after configuring pretended network, while entering STOP2 mode CAN bus didn't go into IDLE state. De-initializing and re-initializing CAN before configuring pretended network fixed this.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 06:41:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SACKERR-causing-reset-during-STOP2-entry-with-CAN-pretended/m-p/1650848#M22952</guid>
      <dc:creator>dinesh_balaji</dc:creator>
      <dc:date>2023-05-16T06:41:48Z</dc:date>
    </item>
  </channel>
</rss>