<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LSPI functions using RTD. in S32K</title>
    <link>https://community.nxp.com/t5/S32K/LSPI-functions-using-RTD/m-p/1650568#M22933</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217297"&gt;@sai-bodhanapu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is an example of LPSPI full-duplex communication included in the RTDs, the Lpspi_Flexio_Ip_S32K312 implements communication between LPSPI2 and FLEXIO_SPI_0.&lt;/P&gt;
&lt;P&gt;It is not the same to use a half-duplex instead of a full-duplex because in full-duplex communication shift registers of both master and slave are linked using two unidirectional lines between MOSI and MISO pins. And in half-duplex for data communication, there is only one data line. The MOSI of the master connects to the MISO of the slave.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
    <pubDate>Mon, 15 May 2023 21:07:20 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2023-05-15T21:07:20Z</dc:date>
    <item>
      <title>LSPI functions using RTD.</title>
      <link>https://community.nxp.com/t5/S32K/LSPI-functions-using-RTD/m-p/1650364#M22927</link>
      <description>&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;I am using S32k312 in S32DS. i need to interface SPI flash memory using RTD. to use RTD LSPI functions i need to use full duplex mode to send and receive data. There is only examples for half duplex mode either for sending or receiving, Can i use Half duplex mode for both sending and recieving the data? i tried that too, it halts at halfduplextransmit function. How can i use RTD drivers for SPI flash please let me know.&lt;/P&gt;&lt;P&gt;Thanking you in advance.&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 13:50:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LSPI-functions-using-RTD/m-p/1650364#M22927</guid>
      <dc:creator>sai-bodhanapu</dc:creator>
      <dc:date>2023-05-15T13:50:43Z</dc:date>
    </item>
    <item>
      <title>Re: LSPI functions using RTD.</title>
      <link>https://community.nxp.com/t5/S32K/LSPI-functions-using-RTD/m-p/1650568#M22933</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217297"&gt;@sai-bodhanapu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is an example of LPSPI full-duplex communication included in the RTDs, the Lpspi_Flexio_Ip_S32K312 implements communication between LPSPI2 and FLEXIO_SPI_0.&lt;/P&gt;
&lt;P&gt;It is not the same to use a half-duplex instead of a full-duplex because in full-duplex communication shift registers of both master and slave are linked using two unidirectional lines between MOSI and MISO pins. And in half-duplex for data communication, there is only one data line. The MOSI of the master connects to the MISO of the slave.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 21:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LSPI-functions-using-RTD/m-p/1650568#M22933</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-05-15T21:07:20Z</dc:date>
    </item>
  </channel>
</rss>