<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K344 MCU Standby Mode Configuration</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1644116#M22581</link>
    <description>Hi YashB, If you call Mcu_SetMode(McuModeSettingConf_Standby), MCU will enter standby mode. I think we can call Mcu_SetMode(McuModeSettingConf_Standby) after generating a event and it is not directedly call Mcu_SetMode(McuModeSettingConf_Standby) after initializing MCU clock. You do not configurate IcuWkpu, so MCU will not wakeup by any event. Thanks! BR, Shunag</description>
    <pubDate>Thu, 04 May 2023 01:49:50 GMT</pubDate>
    <dc:creator>Shuang</dc:creator>
    <dc:date>2023-05-04T01:49:50Z</dc:date>
    <item>
      <title>S32K344 MCU Standby Mode Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1642202#M22490</link>
      <description>&lt;P&gt;Can Anyone share a EB tresos Configurations for S32K344 with Standby Mode Configurations. I am a bit confused at my end. Do i need to configure two modes - RUN and STANDBY ? If possible please share a tresos configuration for the same&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;Can you please help on this?&lt;/P&gt;</description>
      <pubDate>Fri, 28 Apr 2023 10:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1642202#M22490</guid>
      <dc:creator>YashB</dc:creator>
      <dc:date>2023-04-28T10:38:09Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MCU Standby Mode Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1642239#M22492</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216543"&gt;@YashB&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Here are some example:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Have you seen them already?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Fri, 28 Apr 2023 11:32:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1642239#M22492</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-04-28T11:32:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MCU Standby Mode Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1642517#M22502</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt; ,&amp;nbsp;I do not have the RTD v2.0.0 required to view this. Can you send me the link for the same. I am unable to open the links to the S32K344 RTD software , it redirects me to the login page.&lt;/P&gt;</description>
      <pubDate>Sat, 29 Apr 2023 04:17:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1642517#M22502</guid>
      <dc:creator>YashB</dc:creator>
      <dc:date>2023-04-29T04:17:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MCU Standby Mode Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1642532#M22503</link>
      <description>&lt;P&gt;Hello&amp;nbsp; &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did some configuration changes in my existing project.&lt;/P&gt;&lt;P&gt;A short overview of my project- "We are trying to get the NFC 3321 to work with MCU Standby Mode"&lt;/P&gt;&lt;P&gt;So far the NFC&amp;nbsp; chip is working perfectly fine in the RUN mode. I am attaching the project so you can see that we have configured Standby in MCU Mode Configuration in EBTresos.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ideally we have NFC_IRQ that should wake up the system but since NFC chip is powered by GPIO. Is it possible that pin is getting disabled after we run the Standby&amp;nbsp; command in our code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;P.S. Also I was unable to create a support ticket. Is there something wrong on the server side&lt;/P&gt;</description>
      <pubDate>Sat, 29 Apr 2023 12:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1642532#M22503</guid>
      <dc:creator>YashB</dc:creator>
      <dc:date>2023-04-29T12:46:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MCU Standby Mode Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1642657#M22517</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried running the GPIO Wkpu example "S32K344_GPIO_Wkup_S32DS_3_4_RTD_MCAL_2_0" . Since i didn't have the 172 pin EVB, I tried to run it with the&amp;nbsp;&lt;SPAN&gt;S32K3X4EVB-Q257 SCH-47827 REV-A . When I flashed the .elf file onto the HW using Lauterbach in PowerDownRecoverMode , it shows "running(power down)" without even pressing the button to initiate the Standby mode. Also the HW has a min consumption of around 68-70mA, which is not correct.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 01 May 2023 10:44:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1642657#M22517</guid>
      <dc:creator>YashB</dc:creator>
      <dc:date>2023-05-01T10:44:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MCU Standby Mode Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1643521#M22559</link>
      <description>&lt;P&gt;Hi @Danielmartynek, I tried the above projects onto the S32K344 SCH-47827 REV A EVB. I could not get them to run. The GPIO example shows "running (Power Down)" but it doesn't switches to the standby state or the wakeup state using the Push Buttons.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="YashB_1-1683106489824.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/221516i94AC7D22B3C09D0A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="YashB_1-1683106489824.png" alt="YashB_1-1683106489824.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;YashB_1-1683106489824.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/159987"&gt;@jiri_kral&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195919"&gt;@cuongnguyenphu&lt;/a&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 May 2023 09:36:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1643521#M22559</guid>
      <dc:creator>YashB</dc:creator>
      <dc:date>2023-05-03T09:36:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MCU Standby Mode Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1643523#M22560</link>
      <description>&lt;P&gt;Did you get a chance to review this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195919"&gt;@cuongnguyenphu&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/173825"&gt;@Shuang&lt;/a&gt;&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 May 2023 09:40:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1643523#M22560</guid>
      <dc:creator>YashB</dc:creator>
      <dc:date>2023-05-03T09:40:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MCU Standby Mode Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1644116#M22581</link>
      <description>Hi YashB, If you call Mcu_SetMode(McuModeSettingConf_Standby), MCU will enter standby mode. I think we can call Mcu_SetMode(McuModeSettingConf_Standby) after generating a event and it is not directedly call Mcu_SetMode(McuModeSettingConf_Standby) after initializing MCU clock. You do not configurate IcuWkpu, so MCU will not wakeup by any event. Thanks! BR, Shunag</description>
      <pubDate>Thu, 04 May 2023 01:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1644116#M22581</guid>
      <dc:creator>Shuang</dc:creator>
      <dc:date>2023-05-04T01:49:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MCU Standby Mode Configuration</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1645282#M22634</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;A id="link_6" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216543" target="_self" aria-label="View Profile of YashB"&gt;&lt;SPAN class=""&gt;YashB&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;You can check VDD_HV_A current after&amp;nbsp;&lt;SPAN&gt;showing "running (Power Down)"&amp;nbsp;.&amp;nbsp;VDD_HV_A current should be about 60uA&amp;nbsp;&amp;nbsp;after&amp;nbsp;showing "running (Power Down)". If you enable Low-power debug in Trace32,&amp;nbsp;Trace32 debugger will not be automatically disconnect after entering standby mode and will show&amp;nbsp;"running (Power Down)".&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Shuang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 05 May 2023 07:14:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-Standby-Mode-Configuration/m-p/1645282#M22634</guid>
      <dc:creator>Shuang</dc:creator>
      <dc:date>2023-05-05T07:14:12Z</dc:date>
    </item>
  </channel>
</rss>