<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: FlexCAN Reception for only 8 message ID</title>
    <link>https://community.nxp.com/t5/S32K/FlexCAN-Reception-for-only-8-message-ID/m-p/1643475#M22555</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;can you share the code you have?&lt;BR /&gt;CTRL2[RFFN] specifies number of ID filter element used. Be sure that also MCR[MAXMB] is set accordingly.&lt;/P&gt;
&lt;P&gt;Below SDK example show usage of RXFIFO with DMA with 16 filter elements set &lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-RXFIFO-DMA-S32DS-ARM-2018-R1/ta-p/1120014" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-RXFIFO-DMA-S32DS-ARM-2018-R1/ta-p/1120014&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Wed, 03 May 2023 08:29:26 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-05-03T08:29:26Z</dc:date>
    <item>
      <title>FlexCAN Reception for only 8 message ID</title>
      <link>https://community.nxp.com/t5/S32K/FlexCAN-Reception-for-only-8-message-ID/m-p/1643346#M22547</link>
      <description>&lt;P&gt;We are using the S32K118 board, and I have made the following configuration.&lt;BR /&gt;Set the register CAN_MCR[IRMQ] to 0,and set the option of Rx FIFO ID fiters number to 8 Rx FIFO Fiters.The result is that only 8 CAN IDs can be accepted. I would like to accept a quantity of CAN IDs exceeding 8.So I change the number of 8 to 16.But the board can't work of can communication when do this configuration.I have seen some other examples, whether it need to change the number to 40.&lt;BR /&gt;Appreciate any help!&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 03 May 2023 01:58:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlexCAN-Reception-for-only-8-message-ID/m-p/1643346#M22547</guid>
      <dc:creator>xiaobaby22</dc:creator>
      <dc:date>2023-05-03T01:58:16Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN Reception for only 8 message ID</title>
      <link>https://community.nxp.com/t5/S32K/FlexCAN-Reception-for-only-8-message-ID/m-p/1643475#M22555</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;can you share the code you have?&lt;BR /&gt;CTRL2[RFFN] specifies number of ID filter element used. Be sure that also MCR[MAXMB] is set accordingly.&lt;/P&gt;
&lt;P&gt;Below SDK example show usage of RXFIFO with DMA with 16 filter elements set &lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-RXFIFO-DMA-S32DS-ARM-2018-R1/ta-p/1120014" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-RXFIFO-DMA-S32DS-ARM-2018-R1/ta-p/1120014&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 03 May 2023 08:29:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlexCAN-Reception-for-only-8-message-ID/m-p/1643475#M22555</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-05-03T08:29:26Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN Reception for only 8 message ID</title>
      <link>https://community.nxp.com/t5/S32K/FlexCAN-Reception-for-only-8-message-ID/m-p/1649730#M22888</link>
      <description>&lt;P&gt;yeah,I&amp;nbsp;&lt;SPAN&gt;set the option of Rx FIFO ID fiters number to 16 Rx FIFO Fiters.It mean&amp;nbsp;CTRL2[RFFN] (RFFN = 0x01),So the Remaining available maixboxes should begin to MB10.It could be work when I change the number MB8 to MB10.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 14 May 2023 02:42:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlexCAN-Reception-for-only-8-message-ID/m-p/1649730#M22888</guid>
      <dc:creator>xiaobaby22</dc:creator>
      <dc:date>2023-05-14T02:42:05Z</dc:date>
    </item>
  </channel>
</rss>