<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K3 support for IEC 60730 Software Class B</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-support-for-IEC-60730-Software-Class-B/m-p/1642921#M22525</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;S32K3 is automotive device, therefore it is compliant with automotive standards.&lt;/P&gt;
&lt;H5&gt;The S32K3 MCUs of 32/bit AEC-Q100 qualified MCUs combine a scalable family of Arm&lt;SUP&gt;®&lt;/SUP&gt; Cortex&lt;SUP&gt;®&lt;/SUP&gt;-M7-based microcontrollers in single, dual, and lockstep core configurations, supporting up to ASIL D functional safety automotive and industrial applications.&lt;/H5&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Is it possible to implement the IEC 60730 Software Class B on the S32K3?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;I expect that this micro will easily fit any industrial standard as its target is ASIL-D which is most strict automotive one.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;And is there any existing libraries/modules/support for the IEC 60730B tests on the S32K3.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;No direct support for IEC 60730B is available.&lt;/P&gt;
&lt;P&gt;There is SAF (safety application framework) to help customers achive ASIL-D. The micro also has many HW self-test mechanisms in order to achieve safe operation in automotive.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/automotive-software-and-tools/s32-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF" target="_blank"&gt;https://www.nxp.com/design/automotive-software-and-tools/s32-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 02 May 2023 07:18:17 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2023-05-02T07:18:17Z</dc:date>
    <item>
      <title>S32K3 support for IEC 60730 Software Class B</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-support-for-IEC-60730-Software-Class-B/m-p/1642829#M22519</link>
      <description>&lt;P&gt;Hi there,&amp;nbsp;&lt;/P&gt;&lt;P&gt;We'd love to make use of the&amp;nbsp;S32K3 in our next generation of products.&amp;nbsp;Some of our existing customers require the products to be IEC 60730 Software Class B compliant.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to implement the&amp;nbsp;IEC 60730 Software Class B on the&amp;nbsp;S32K3? And is there any existing libraries/modules/support for the IEC 60730B tests on the&amp;nbsp;S32K3.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If not, any suggestions would be appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&amp;nbsp;&lt;BR /&gt;Jason&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 May 2023 02:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-support-for-IEC-60730-Software-Class-B/m-p/1642829#M22519</guid>
      <dc:creator>JasonG</dc:creator>
      <dc:date>2023-05-02T02:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 support for IEC 60730 Software Class B</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-support-for-IEC-60730-Software-Class-B/m-p/1642921#M22525</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;S32K3 is automotive device, therefore it is compliant with automotive standards.&lt;/P&gt;
&lt;H5&gt;The S32K3 MCUs of 32/bit AEC-Q100 qualified MCUs combine a scalable family of Arm&lt;SUP&gt;®&lt;/SUP&gt; Cortex&lt;SUP&gt;®&lt;/SUP&gt;-M7-based microcontrollers in single, dual, and lockstep core configurations, supporting up to ASIL D functional safety automotive and industrial applications.&lt;/H5&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Is it possible to implement the IEC 60730 Software Class B on the S32K3?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;I expect that this micro will easily fit any industrial standard as its target is ASIL-D which is most strict automotive one.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;And is there any existing libraries/modules/support for the IEC 60730B tests on the S32K3.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;No direct support for IEC 60730B is available.&lt;/P&gt;
&lt;P&gt;There is SAF (safety application framework) to help customers achive ASIL-D. The micro also has many HW self-test mechanisms in order to achieve safe operation in automotive.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/automotive-software-and-tools/s32-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF" target="_blank"&gt;https://www.nxp.com/design/automotive-software-and-tools/s32-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 May 2023 07:18:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-support-for-IEC-60730-Software-Class-B/m-p/1642921#M22525</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-05-02T07:18:17Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 support for IEC 60730 Software Class B</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-support-for-IEC-60730-Software-Class-B/m-p/1646854#M22728</link>
      <description>Hi Peter,&lt;BR /&gt;&lt;BR /&gt;Thank you for your response. That is great to hear that there is at least some pathway to support the standard.&lt;BR /&gt;&lt;BR /&gt;Kind regards,&lt;BR /&gt;Jason</description>
      <pubDate>Tue, 09 May 2023 06:54:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-support-for-IEC-60730-Software-Class-B/m-p/1646854#M22728</guid>
      <dc:creator>JasonG</dc:creator>
      <dc:date>2023-05-09T06:54:15Z</dc:date>
    </item>
  </channel>
</rss>