<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 s32k148 EVB QSPI program error</title>
    <link>https://community.nxp.com/t5/S32K/s32k148-EVB-QSPI-program-error/m-p/1642254#M22493</link>
    <description>&lt;P&gt;Hello NXP community,&lt;/P&gt;&lt;P&gt;I have some problems with the QSPI programming functions provided by the 'FLASH_MX25L6433F_DRV' drivers. When I try to program from 1 to 192 Bytes or 256 Bytes to QSPI everything works fine, but when I try to program from any quantity of bytes between 193 to 255 Bytes with a single command the function returns an erroneous status that I don't know what it is due to.&lt;/P&gt;&lt;P&gt;I am using the S32K148 EVB evaluation board and the example project 'qspi_external_flash_s32k148'.&lt;/P&gt;&lt;P&gt;Any idea what causes this error?&lt;/P&gt;</description>
    <pubDate>Fri, 28 Apr 2023 12:21:10 GMT</pubDate>
    <dc:creator>FBS</dc:creator>
    <dc:date>2023-04-28T12:21:10Z</dc:date>
    <item>
      <title>s32k148 EVB QSPI program error</title>
      <link>https://community.nxp.com/t5/S32K/s32k148-EVB-QSPI-program-error/m-p/1642254#M22493</link>
      <description>&lt;P&gt;Hello NXP community,&lt;/P&gt;&lt;P&gt;I have some problems with the QSPI programming functions provided by the 'FLASH_MX25L6433F_DRV' drivers. When I try to program from 1 to 192 Bytes or 256 Bytes to QSPI everything works fine, but when I try to program from any quantity of bytes between 193 to 255 Bytes with a single command the function returns an erroneous status that I don't know what it is due to.&lt;/P&gt;&lt;P&gt;I am using the S32K148 EVB evaluation board and the example project 'qspi_external_flash_s32k148'.&lt;/P&gt;&lt;P&gt;Any idea what causes this error?&lt;/P&gt;</description>
      <pubDate>Fri, 28 Apr 2023 12:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k148-EVB-QSPI-program-error/m-p/1642254#M22493</guid>
      <dc:creator>FBS</dc:creator>
      <dc:date>2023-04-28T12:21:10Z</dc:date>
    </item>
    <item>
      <title>Re: s32k148 EVB QSPI program error</title>
      <link>https://community.nxp.com/t5/S32K/s32k148-EVB-QSPI-program-error/m-p/1646965#M22736</link>
      <description>&lt;P&gt;Could you specify used RTD/SDK and S32DS versions?&lt;/P&gt;</description>
      <pubDate>Tue, 09 May 2023 08:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k148-EVB-QSPI-program-error/m-p/1646965#M22736</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-05-09T08:38:55Z</dc:date>
    </item>
    <item>
      <title>Re: s32k148 EVB QSPI program error</title>
      <link>https://community.nxp.com/t5/S32K/s32k148-EVB-QSPI-program-error/m-p/1647941#M22786</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52613"&gt;@davidtosenovjan&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sure&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;S32DS 3.4 version&lt;/LI&gt;&lt;LI&gt;S32k148_SDK 4.0.2 version&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;The specific function I am referring to is the following&lt;/P&gt;&lt;P&gt;/*!&lt;BR /&gt;* @brief Writes data in serial flash&lt;BR /&gt;*&lt;BR /&gt;* @param instance QuadSPI peripheral instance number&lt;BR /&gt;* @param address Start address of area to be programmed&lt;BR /&gt;* @param data Data to be programmed in flash&lt;BR /&gt;* @param size Size of data buffer&lt;BR /&gt;* @return Error or success status returned by API&lt;BR /&gt;*/&lt;BR /&gt;status_t FLASH_MX25L6433F_DRV_Program(uint32_t instance, uint32_t address, const uint8_t * data, uint32_t size);&lt;/P&gt;</description>
      <pubDate>Wed, 10 May 2023 12:22:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k148-EVB-QSPI-program-error/m-p/1647941#M22786</guid>
      <dc:creator>FBS</dc:creator>
      <dc:date>2023-05-10T12:22:57Z</dc:date>
    </item>
    <item>
      <title>Re: s32k148 EVB QSPI program error</title>
      <link>https://community.nxp.com/t5/S32K/s32k148-EVB-QSPI-program-error/m-p/1663418#M23612</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52613"&gt;@davidtosenovjan&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Any news about it?&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jun 2023 10:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k148-EVB-QSPI-program-error/m-p/1663418#M23612</guid>
      <dc:creator>FBS</dc:creator>
      <dc:date>2023-06-05T10:41:27Z</dc:date>
    </item>
  </channel>
</rss>