<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: VLPS differences S32K144 and S32K146 ? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/VLPS-differences-S32K144-and-S32K146/m-p/764573#M2233</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;As per S32K1xx Datasheet, the consumption in VLPS of S32K146 is slightly higher (+20uA, Table 7 of DS) than the consumption of S32K144.&lt;BR /&gt;5mA is really too much. &lt;BR /&gt;The board must run stand-alone without debugger to enter VLPS.&lt;BR /&gt;Can you check VLPSA bit? Do you drive any external load?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Apr 2018 11:17:07 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-04-06T11:17:07Z</dc:date>
    <item>
      <title>VLPS differences S32K144 and S32K146 ?</title>
      <link>https://community.nxp.com/t5/S32K/VLPS-differences-S32K144-and-S32K146/m-p/764572#M2232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear support team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there some differences between the S32K144 and S32K146 very low power mode (VLPS)&amp;nbsp;?&lt;/P&gt;&lt;P&gt;I use this sequence to go to very low power mode:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;During the initialization:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I set SMC_PMPROT_AVLP to 1&lt;/LI&gt;&lt;LI&gt;I set SMC_PMCTRL_STOPM to 2&lt;/LI&gt;&lt;LI&gt;I set SMC_STOPCTRL_STOPO to 0&lt;/LI&gt;&lt;LI&gt;I set SCB_SCR_SLEEPDEEP to 1&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;When I want to to go very low power mode:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I switch off the unused peripherals (PCC registers)&lt;/LI&gt;&lt;LI&gt;I start my wake up timer (LPTMR)&lt;/LI&gt;&lt;LI&gt;I execute the WFI instruction&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With my hardware with S32K146, the current consumption in sleep mode is 5mA higher than with the other hardware (with S32K144).&lt;/P&gt;&lt;P&gt;is this normal that the S32K146 consumes 5mA more than the S32K144 (in VLPS or RUN mode) ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 08:21:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/VLPS-differences-S32K144-and-S32K146/m-p/764572#M2232</guid>
      <dc:creator>stabilo</dc:creator>
      <dc:date>2018-04-04T08:21:59Z</dc:date>
    </item>
    <item>
      <title>Re: VLPS differences S32K144 and S32K146 ?</title>
      <link>https://community.nxp.com/t5/S32K/VLPS-differences-S32K144-and-S32K146/m-p/764573#M2233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;As per S32K1xx Datasheet, the consumption in VLPS of S32K146 is slightly higher (+20uA, Table 7 of DS) than the consumption of S32K144.&lt;BR /&gt;5mA is really too much. &lt;BR /&gt;The board must run stand-alone without debugger to enter VLPS.&lt;BR /&gt;Can you check VLPSA bit? Do you drive any external load?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2018 11:17:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/VLPS-differences-S32K144-and-S32K146/m-p/764573#M2233</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-04-06T11:17:07Z</dc:date>
    </item>
  </channel>
</rss>