<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K144 CAN Failed</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-CAN-Failed/m-p/1636900#M22259</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;unfortunately from this values nothing can be said.&lt;BR /&gt;Once error interrupt happens you should read ESR1&amp;nbsp;to capture all error condition and status bits. This action clears the respective bits that were set since the last read access. Read ECR as well.&lt;BR /&gt;Module only enters bus off when is sending a messages and errors are detected, it follows rules described in CAN protocol.&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Thu, 20 Apr 2023 05:25:14 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-04-20T05:25:14Z</dc:date>
    <item>
      <title>S32K144 CAN Failed</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-Failed/m-p/1634153#M22146</link>
      <description>&lt;P&gt;Now my design is TI MCU+ S32K144. TI is master, S32K144 is slave.&lt;/P&gt;&lt;P&gt;At the begining, The can works normally. After about fifteen hours, the CAN failed.&lt;/P&gt;&lt;P&gt;The measured waveform of S32K144 TX is shown below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wenfengyao_0-1681526421687.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219353iFA7C7E8EA8445147/image-size/medium?v=v2&amp;amp;px=400" role="button" title="wenfengyao_0-1681526421687.png" alt="wenfengyao_0-1681526421687.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In addition, this waveform is also generated on TX when writing a program to S32K144.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do you have any directions?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 15 Apr 2023 02:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-Failed/m-p/1634153#M22146</guid>
      <dc:creator>wenfengyao</dc:creator>
      <dc:date>2023-04-15T02:43:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 CAN Failed</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-Failed/m-p/1634552#M22161</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;at which condition this signal is taken? When TI MCU is sending a message, or S32K144 is trying to do that? How is the CAN connection done between MCU's.&lt;BR /&gt;If you see issue in communication, check if device detect any king of error, so read ESR1/ECR registers.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 17 Apr 2023 09:37:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-Failed/m-p/1634552#M22161</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-04-17T09:37:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 CAN Failed</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-Failed/m-p/1636867#M22257</link>
      <description>&lt;P class=""&gt;The MCU is all sending and receiving messages, connected through CAN OE&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Now I have added the CAN bus off interrupt to the program. When CAN enters bus off, stop the current send and clear the error flag.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;At present, there is no previous phenomenon, but it is still not clear why CAN communication failure&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wenfengyao_0-1681961229495.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219983i38D122001F2E546A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="wenfengyao_0-1681961229495.jpeg" alt="wenfengyao_0-1681961229495.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 03:32:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-Failed/m-p/1636867#M22257</guid>
      <dc:creator>wenfengyao</dc:creator>
      <dc:date>2023-04-20T03:32:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 CAN Failed</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-CAN-Failed/m-p/1636900#M22259</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;unfortunately from this values nothing can be said.&lt;BR /&gt;Once error interrupt happens you should read ESR1&amp;nbsp;to capture all error condition and status bits. This action clears the respective bits that were set since the last read access. Read ECR as well.&lt;BR /&gt;Module only enters bus off when is sending a messages and errors are detected, it follows rules described in CAN protocol.&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 05:25:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-CAN-Failed/m-p/1636900#M22259</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-04-20T05:25:14Z</dc:date>
    </item>
  </channel>
</rss>