<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ADC accuracy in S32K</title>
    <link>https://community.nxp.com/t5/S32K/ADC-accuracy/m-p/763340#M2220</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;you wrote the voltage is 0-36V. I guess there’s resistor voltage divider, right? If so, what is the resistance? If it is too high, the error can be caused by input leakage offset error. Take a look at this application note, page 14:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN2438.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN2438.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Lukas&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Feb 2018 12:05:31 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2018-02-21T12:05:31Z</dc:date>
    <item>
      <title>ADC accuracy</title>
      <link>https://community.nxp.com/t5/S32K/ADC-accuracy/m-p/763339#M2219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear support team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the ADC0 of&amp;nbsp;the S32K144&amp;nbsp;to measure&amp;nbsp;voltage (0 to 36V).&lt;/P&gt;&lt;P&gt;The ADC channel is configured to measure continuously at a sample rate of 5µs.&amp;nbsp; DMA transfer are triggered to transfer 32 ADC measurement into the buffer. Then, filtering and conversions are performed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two problems:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The raw values into the buffer vary a lot (constant noise of ~&amp;nbsp;15 digits)&lt;/LI&gt;&lt;LI&gt;The final voltage measured (filtered) is not accurate enough:&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18508iBDCBB0BF3746FFB2/image-size/large?v=v2&amp;amp;px=999" title="Accuracy.JPG" alt="Accuracy.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This picture shows the absolute error in function of the input voltage. Each point on the graph is a mean of 10 measurements (on these 10 measurement, the noise on measured values never exceed 5mV). As you can see, the error is very random (e.g. +40mV at 25.0V, -30mV at 26.0V).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to enable the ADC self calibration, and the results are even worse.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea on how to improve my measurement accuracy ? (measurement rate&amp;nbsp;?&amp;nbsp;reference voltage ? analog input capacitor ?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope you can help,&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Feb 2018 17:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-accuracy/m-p/763339#M2219</guid>
      <dc:creator>stabilo</dc:creator>
      <dc:date>2018-02-20T17:21:39Z</dc:date>
    </item>
    <item>
      <title>Re: ADC accuracy</title>
      <link>https://community.nxp.com/t5/S32K/ADC-accuracy/m-p/763340#M2220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;you wrote the voltage is 0-36V. I guess there’s resistor voltage divider, right? If so, what is the resistance? If it is too high, the error can be caused by input leakage offset error. Take a look at this application note, page 14:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN2438.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN2438.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Lukas&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Feb 2018 12:05:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-accuracy/m-p/763340#M2220</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2018-02-21T12:05:31Z</dc:date>
    </item>
  </channel>
</rss>