<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32DS Change processor type</title>
    <link>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635279#M22188</link>
    <description>&lt;P&gt;&lt;A href="mailto:Hi@koehlerl" target="_blank"&gt;Hi@koehlerl&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Can you take a screenshot?&lt;BR /&gt;In fact, this operation is not very convenient, and some files need to be deleted and added. I suggest to create a new S32K146 project directly, and refer to the configuration of the old project. This work is very simple and there will be no accidental errors.&lt;/P&gt;</description>
    <pubDate>Tue, 18 Apr 2023 09:04:07 GMT</pubDate>
    <dc:creator>Senlent</dc:creator>
    <dc:date>2023-04-18T09:04:07Z</dc:date>
    <item>
      <title>S32DS Change processor type</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635134#M22183</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;In my project I changed the processor type from S32K144 to S32K146.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;It all worked until I can't change the SDK.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In the SDK path in the project tree is the right S32K146 MCU.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="koehlerl_0-1681799930670.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219547iEC35326215379093/image-size/medium?v=v2&amp;amp;px=400" role="button" title="koehlerl_0-1681799930670.png" alt="koehlerl_0-1681799930670.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;koehlerl_0-1681799930670.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I also have changed the defined symbols for preprocessor.&lt;/P&gt;&lt;P&gt;But I can't chnage the SDK in the Project settings:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="koehlerl_1-1681800188133.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219550i55725BF8EC2F1DA2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="koehlerl_1-1681800188133.png" alt="koehlerl_1-1681800188133.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;koehlerl_1-1681800188133.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The symbol means:&lt;/P&gt;&lt;P&gt;SDK does not support processor or core required by the project. Cannot attach.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What do I have to do to be able to change the SDK in the project settimgs?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Lutz&lt;/P&gt;</description>
      <pubDate>Tue, 18 Apr 2023 06:52:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635134#M22183</guid>
      <dc:creator>koehlerl</dc:creator>
      <dc:date>2023-04-18T06:52:43Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Change processor type</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635171#M22184</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@koehlerl" target="_blank"&gt;Hi@koehlerl&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;please refer to this post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Change-the-CPU-Derivative-in-an-SDK-Based-Application/ta-p/1112149" target="_self"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Change-the-CPU-Derivative-in-an-SDK-Based-Application/ta-p/1112149&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;hope it can helps you!&lt;/P&gt;</description>
      <pubDate>Tue, 18 Apr 2023 07:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635171#M22184</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-04-18T07:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Change processor type</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635269#M22186</link>
      <description>&lt;P&gt;I have done all the steps from post&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Change-the-CPU-Derivative-in-an-SDK-Based-Application/ta-p/1112149" target="_self"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Change-the-CPU-Derivative-in-an-...&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;and the project works &lt;STRONG&gt;but the sdk project setting is not right respectively I cannot attach to S32K146.&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR Lutz&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Apr 2023 08:52:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635269#M22186</guid>
      <dc:creator>koehlerl</dc:creator>
      <dc:date>2023-04-18T08:52:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Change processor type</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635279#M22188</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@koehlerl" target="_blank"&gt;Hi@koehlerl&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Can you take a screenshot?&lt;BR /&gt;In fact, this operation is not very convenient, and some files need to be deleted and added. I suggest to create a new S32K146 project directly, and refer to the configuration of the old project. This work is very simple and there will be no accidental errors.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Apr 2023 09:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635279#M22188</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-04-18T09:04:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Change processor type</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635326#M22193</link>
      <description>&lt;P&gt;The sreenshot&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="koehlerl_0-1681810843276.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219623i18D4D4AD852D10E6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="koehlerl_0-1681810843276.png" alt="koehlerl_0-1681810843276.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;koehlerl_0-1681810843276.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I cannot attach the S32K146&lt;/P&gt;</description>
      <pubDate>Tue, 18 Apr 2023 09:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635326#M22193</guid>
      <dc:creator>koehlerl</dc:creator>
      <dc:date>2023-04-18T09:41:10Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Change processor type</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635364#M22196</link>
      <description>&lt;P&gt;Hi@koehlerl&lt;/P&gt;
&lt;P&gt;I reproduced it, it is indeed like this, this really cannot be changed&lt;BR /&gt;But this does not affect the compilation of the project, I think this is not a bug,&lt;/P&gt;</description>
      <pubDate>Tue, 18 Apr 2023 10:38:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-Change-processor-type/m-p/1635364#M22196</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-04-18T10:38:33Z</dc:date>
    </item>
  </channel>
</rss>