<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Tresos example project for S32K148</title>
    <link>https://community.nxp.com/t5/S32K/Tresos-example-project-for-S32K148/m-p/1634568#M22165</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Sample application are for example in S32K14X_MCAL4_0_RTM_1_0_4 and there are correct versions.&lt;/P&gt;
&lt;P&gt;If you want to use 1.0.0 you will need to replace it with correct version. (0.9.0. in this case) - I didn't seen it available.&lt;/P&gt;
&lt;P&gt;The examples for&amp;nbsp;SW32K1_RTD_4.4_1.0.1 are located in:&lt;/P&gt;
&lt;P&gt;:\NXP\SW32K1_RTD_4.4_1.0.1\eclipse\plugins\Adc_TS_T40D2M10I1R0\examples\EBT\Adc_example_S32K148&lt;/P&gt;
&lt;P&gt;Similar in folders for each driver.&lt;/P&gt;
&lt;P&gt;For the beginning I would recommend to use RTD (real time drivers) instead of MCAL.&lt;/P&gt;
&lt;P&gt;There are much more examples.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt; &lt;/LI-WRAPPER&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 17 Apr 2023 09:58:17 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2023-04-17T09:58:17Z</dc:date>
    <item>
      <title>Tresos example project for S32K148</title>
      <link>https://community.nxp.com/t5/S32K/Tresos-example-project-for-S32K148/m-p/1631959#M22021</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I couldn`t find any example project for Tresos. I have download several MCAL versions to check this. Inside of installation folder for MCALs(C:\NXP\AUTOSAR\S32K1XX_MCAL4_0_RTM_1_0_5) there is no example project. Only the plugins available.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; It is same situation for RTD, it has only plugins there is no example. How can I find the Tresos example for S32K148?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 08:46:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tresos-example-project-for-S32K148/m-p/1631959#M22021</guid>
      <dc:creator>drsn</dc:creator>
      <dc:date>2023-04-12T08:46:00Z</dc:date>
    </item>
    <item>
      <title>Re: Tresos example project for S32K148</title>
      <link>https://community.nxp.com/t5/S32K/Tresos-example-project-for-S32K148/m-p/1632120#M22032</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Hmm, that is strange.&lt;/P&gt;
&lt;P&gt;I have just installed version S32K14Xx_MCAL4_0_RTM_1_0_0 and sample application is there:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1681300834814.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/218938i56CAD4F06EDB5D6A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="petervlna_0-1681300834814.png" alt="petervlna_0-1681300834814.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Usually the sample applications are in the base releases.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 12:01:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tresos-example-project-for-S32K148/m-p/1632120#M22032</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-04-12T12:01:38Z</dc:date>
    </item>
    <item>
      <title>Re: Tresos example project for S32K148</title>
      <link>https://community.nxp.com/t5/S32K/Tresos-example-project-for-S32K148/m-p/1632158#M22036</link>
      <description>&lt;P&gt;Hi Peter,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Thank you for the answer. Yes sample application is only available in base version. but now I have a problem while opening the project in Tresos. sample project uses "xxx_TS_T40D2M9I0R0" version plugins but I have&amp;nbsp;"xxx_TS_T40D2M10I0R0" with base version. It seems that sample project is using older version. Do you know where can I find this version?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 13:01:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tresos-example-project-for-S32K148/m-p/1632158#M22036</guid>
      <dc:creator>drsn</dc:creator>
      <dc:date>2023-04-12T13:01:20Z</dc:date>
    </item>
    <item>
      <title>Re: Tresos example project for S32K148</title>
      <link>https://community.nxp.com/t5/S32K/Tresos-example-project-for-S32K148/m-p/1634568#M22165</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Sample application are for example in S32K14X_MCAL4_0_RTM_1_0_4 and there are correct versions.&lt;/P&gt;
&lt;P&gt;If you want to use 1.0.0 you will need to replace it with correct version. (0.9.0. in this case) - I didn't seen it available.&lt;/P&gt;
&lt;P&gt;The examples for&amp;nbsp;SW32K1_RTD_4.4_1.0.1 are located in:&lt;/P&gt;
&lt;P&gt;:\NXP\SW32K1_RTD_4.4_1.0.1\eclipse\plugins\Adc_TS_T40D2M10I1R0\examples\EBT\Adc_example_S32K148&lt;/P&gt;
&lt;P&gt;Similar in folders for each driver.&lt;/P&gt;
&lt;P&gt;For the beginning I would recommend to use RTD (real time drivers) instead of MCAL.&lt;/P&gt;
&lt;P&gt;There are much more examples.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt; &lt;/LI-WRAPPER&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 17 Apr 2023 09:58:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Tresos-example-project-for-S32K148/m-p/1634568#M22165</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-04-17T09:58:17Z</dc:date>
    </item>
  </channel>
</rss>