<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN Debug problem in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CAN-Debug-problem/m-p/1633146#M22083</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;after RXFIFO table is configured, check content of MCR, CTRL2, RXIMRx registers and ID table area. Is there all as expected?&lt;BR /&gt;Do you have properly set RXIMR register to have bit30 set so IDE bit is compared?&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Thu, 13 Apr 2023 12:15:22 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-04-13T12:15:22Z</dc:date>
    <item>
      <title>CAN Debug problem</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Debug-problem/m-p/1632822#M22062</link>
      <description>&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;One of the problems I encountered during debugging was to select filter mode A and call the FlexCAN_Ip_ConfigRxFifo function. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;0x00F00000 is set in the incoming configuration table, extending frame.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; Extended frames can be received normally, but standard frames can also be received.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;If isExtendedFrame is true, it can receive extended frames of 0x00F00000 and standard frames of 0x3C. If isExtendedFrame is false, set 0x00F00000 and no data will come in&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="7b774ccdec7034974bea74d1d240d2b.png" style="width: 305px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219036i5E1645821C956CDE/image-size/large?v=v2&amp;amp;px=999" role="button" title="7b774ccdec7034974bea74d1d240d2b.png" alt="7b774ccdec7034974bea74d1d240d2b.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="201c7aa55b9f33c738bcbe859f39ca8.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219037i89696B57E3049D1B/image-size/large?v=v2&amp;amp;px=999" role="button" title="201c7aa55b9f33c738bcbe859f39ca8.png" alt="201c7aa55b9f33c738bcbe859f39ca8.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Apr 2023 06:15:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Debug-problem/m-p/1632822#M22062</guid>
      <dc:creator>yiguangtang</dc:creator>
      <dc:date>2023-04-13T06:15:55Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Debug problem</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Debug-problem/m-p/1633146#M22083</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;after RXFIFO table is configured, check content of MCR, CTRL2, RXIMRx registers and ID table area. Is there all as expected?&lt;BR /&gt;Do you have properly set RXIMR register to have bit30 set so IDE bit is compared?&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 13 Apr 2023 12:15:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Debug-problem/m-p/1633146#M22083</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-04-13T12:15:22Z</dc:date>
    </item>
  </channel>
</rss>