<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K148 RTD Example/Use cases Projects</title>
    <link>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1633069#M22079</link>
    <description>&lt;P&gt;Go to &lt;A href="https://nxp1.sharepoint.com/:u:/r/teams/25_66/Shared%20Documents/2022%20GPIS%20AE%20Project/S32K1_RTD_UseCase/Release/S32K148_EVB_RTD101_UseCase.7z?csf=1&amp;amp;web=1&amp;amp;e=FNhKz9" target="_self"&gt;here&lt;/A&gt; to get the software package.&lt;/P&gt;</description>
    <pubDate>Thu, 13 Apr 2023 10:08:35 GMT</pubDate>
    <dc:creator>StephenDu</dc:creator>
    <dc:date>2023-04-13T10:08:35Z</dc:date>
    <item>
      <title>S32K148 RTD Example/Use cases Projects</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1633067#M22078</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200218"&gt;@S32kUser&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Due to the discontinuation of updates to MCAL and SDK, it is recommended that users use new RTD software. Although the RTD software provides many example projects by default, the default project focuses on demonstrating the basic functions of peripherals. In addition, some customers hope for the development method of MCAL+S32DS, so we provide a new software package. This software package is configured with EBT, compiling, and debugging with S32DS. And fully collect customer needs, this package focuses on some practical use cases.&lt;/P&gt;
&lt;P&gt;Here &lt;SPAN class="fontstyle0"&gt;summarize all the use cases’ features, For more detailed information, please refer to the&lt;BR /&gt;description of each project:&lt;/SPAN&gt;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_Basic:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This is a basic template project, you can create a new project based on it quickly. It includes the&lt;BR /&gt;EBT and S32DS project.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_AdcMultiCHPdbDma:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This project shows how to use multiple ADC channels triggered by the PDB, the data&lt;BR /&gt;transmission with DMA. It was implemented by an ADC group. The Adc0Group0 executes a software triggered a Single One-Shot Normal conversion chain and the data will be read by polling. The group contains S28(Ch44) | VREFH(CH29) | VREFL(CH30) | Bandgap(CH27) channels.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_BootApp:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This project shows a fully functional bootloader &amp;amp; application solution. It mainly includes TP(ISO&lt;BR /&gt;15765-2), UDS(ISO-14229) and necessary driver modules and so on.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_CanLinEthernet:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This example demonstrates the usage of the communication interface: CAN(FD)/LIN/ETH. For the&lt;BR /&gt;CAN(FD) example, it use the CAN0 channel, and work in interrupt mode, it will send out the&lt;BR /&gt;message when it received any message. For the LIN example, it provided a test *.ldf file. And it will control the LED. For the ETH example, the MAC work in loopback mode, it will send out a frame then it will generate the receive interrupt.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_CryptoEep:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;In this example project, it performs a synchronous encryption/decryption operations with a pair of&lt;BR /&gt;key and plain/cipher texts.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_FeeVersionControl:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This example shows two solutions, one is Fee version control strategy for the situation in which not include NVRAM. And another feature is that the ECC error process guidance.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_FlsAC:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This project mainly to show the usage of Access Code (AC) of FLS module. This feature often used in the bootloader/OTA case.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_FlsQspi:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This project mainly shows how to configure and how to use the external QSPI flash (MX25L6433).&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_FreeMASTER:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This example demonstrates the usage of the FreeMaster. It supports both UART and CAN bus&lt;BR /&gt;interfaces, you can select it according to your requirement.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_FreeRTOS:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This project to show the usage of FreeRTOS. Three tasks created. One of the tasks responsible for initialize the peripheral, one of the task process the button logic action, and the other one control led.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_InputCapture:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This project show the usage of “Edge Count mode” based on FTM0 and the usage of “Signal&lt;BR /&gt;Measurement” to detect period/duty time based on FTM1.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_PwmPhaseShift:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This project shows the configuration of PWM phase shift. Two pairs of PWM channels(total four&lt;BR /&gt;pins) are configured to simulate the motor control signal (Just show the H-Bridge signal, not to real&lt;BR /&gt;control a motor).&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_SafetySoftware:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This example demonstrates Safety Mechanism(SM) for Failure mode. It provides rich safety&lt;BR /&gt;policies, please refer to the project description for detailed information.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_StandbyWakeup:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This example show you how to configure and use the wake-up source. Three wake-up sources are configured: RTC, IRQ(BTN:SW4), CAN Bus.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;&lt;SPAN class="fontstyle2"&gt;&lt;STRONG&gt;K148_RTD101_SysVoltageMonitor:&lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class="fontstyle3"&gt;This example shows the Low voltage monitoring use case. Due to the EVB don't have specify low&lt;BR /&gt;voltage detect circuit, we use the external SBC to monitor the voltage, when low voltage detected, it will generate a interrupt to MCU by a pin.&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/LI&gt;
&lt;/UL&gt;</description>
      <pubDate>Thu, 13 Apr 2023 10:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1633067#M22078</guid>
      <dc:creator>StephenDu</dc:creator>
      <dc:date>2023-04-13T10:04:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 RTD Example/Use cases Projects</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1633069#M22079</link>
      <description>&lt;P&gt;Go to &lt;A href="https://nxp1.sharepoint.com/:u:/r/teams/25_66/Shared%20Documents/2022%20GPIS%20AE%20Project/S32K1_RTD_UseCase/Release/S32K148_EVB_RTD101_UseCase.7z?csf=1&amp;amp;web=1&amp;amp;e=FNhKz9" target="_self"&gt;here&lt;/A&gt; to get the software package.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Apr 2023 10:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1633069#M22079</guid>
      <dc:creator>StephenDu</dc:creator>
      <dc:date>2023-04-13T10:08:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 RTD Example/Use cases Projects</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1665968#M23743</link>
      <description>&lt;P&gt;Hi@&lt;A id="link_7" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/120987" target="_self" aria-label="View Profile of nxf50137"&gt;&lt;SPAN class=""&gt;nxf50137&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hi,Stephen,thanks for sharing.&lt;/P&gt;
&lt;P&gt;But this link cannot be opened, we and all customers do not have access rights, can we publish it directly?&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 07:45:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1665968#M23743</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-06-08T07:45:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 RTD Example/Use cases Projects</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1666105#M23749</link>
      <description>&lt;P&gt;hi, Senlent&lt;/P&gt;&lt;P&gt;Sorry bring you a trouble. Due to the community has limitation for the package size. I can't attach it here directly. I didn't find you in the teams, can you ping me in teams or email to me, I can add you in the list. Or you can contact FAE teams, they also have the access to it.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 10:21:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1666105#M23749</guid>
      <dc:creator>StephenDu</dc:creator>
      <dc:date>2023-06-08T10:21:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 RTD Example/Use cases Projects</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1700670#M25839</link>
      <description>&lt;P&gt;Thank you for raising the access concern! Were you guys able to find a way to make those large files available for us the customers?&lt;/P&gt;</description>
      <pubDate>Tue, 08 Aug 2023 04:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1700670#M25839</guid>
      <dc:creator>andreybe</dc:creator>
      <dc:date>2023-08-08T04:31:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 RTD Example/Use cases Projects</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1700741#M25842</link>
      <description>&lt;P&gt;hi, all&lt;/P&gt;
&lt;P&gt;Please refer to the attached package:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Aug 2023 06:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1700741#M25842</guid>
      <dc:creator>StephenDu</dc:creator>
      <dc:date>2023-08-08T06:14:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 RTD Example/Use cases Projects</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1788702#M30653</link>
      <description>Hello, I don't have access to the file. Is there another way to access these examples?&lt;BR /&gt;&lt;BR /&gt;Thank you</description>
      <pubDate>Mon, 15 Jan 2024 09:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-RTD-Example-Use-cases-Projects/m-p/1788702#M30653</guid>
      <dc:creator>amZ1</dc:creator>
      <dc:date>2024-01-15T09:47:52Z</dc:date>
    </item>
  </channel>
</rss>