<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックUART0 problem for S32K358</title>
    <link>https://community.nxp.com/t5/S32K/UART0-problem-for-S32K358/m-p/1632869#M22066</link>
    <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;I met a problem about UART0 debug of S32K358.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We use S32K358 instead of S32K344 on the board. PTA2 is set as LPUART0_RX function and PTA2 is set as&amp;nbsp;LPUART0_TX function. But now&amp;nbsp;LPUART0_RX doesn't work. MCU can't receive any data from PTA2. But LPUART0_TX works fine. It can output logs from MCU. Are S32K358 and S32K344&amp;nbsp;pin to pin? UART0 of S32K344 works fine with the same setting.&lt;/P&gt;&lt;P&gt;Looking forward to your reply. Thanks.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 13 Apr 2023 06:54:13 GMT</pubDate>
    <dc:creator>CathyX</dc:creator>
    <dc:date>2023-04-13T06:54:13Z</dc:date>
    <item>
      <title>UART0 problem for S32K358</title>
      <link>https://community.nxp.com/t5/S32K/UART0-problem-for-S32K358/m-p/1632869#M22066</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;I met a problem about UART0 debug of S32K358.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We use S32K358 instead of S32K344 on the board. PTA2 is set as LPUART0_RX function and PTA2 is set as&amp;nbsp;LPUART0_TX function. But now&amp;nbsp;LPUART0_RX doesn't work. MCU can't receive any data from PTA2. But LPUART0_TX works fine. It can output logs from MCU. Are S32K358 and S32K344&amp;nbsp;pin to pin? UART0 of S32K344 works fine with the same setting.&lt;/P&gt;&lt;P&gt;Looking forward to your reply. Thanks.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Apr 2023 06:54:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/UART0-problem-for-S32K358/m-p/1632869#M22066</guid>
      <dc:creator>CathyX</dc:creator>
      <dc:date>2023-04-13T06:54:13Z</dc:date>
    </item>
    <item>
      <title>Re: UART0 problem for S32K358</title>
      <link>https://community.nxp.com/t5/S32K/UART0-problem-for-S32K358/m-p/1633218#M22085</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191296"&gt;@CathyX&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Yes, the pinout are pin-to-pin compatible.&lt;/P&gt;
&lt;P&gt;Have you tried more boards? There can be an HW issue.&lt;/P&gt;
&lt;P&gt;Was the SW for both MCUs built with the same drivers?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 13 Apr 2023 14:13:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/UART0-problem-for-S32K358/m-p/1633218#M22085</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-04-13T14:13:59Z</dc:date>
    </item>
  </channel>
</rss>