<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRegarding S32K142 Bootloader using PCAN</title>
    <link>https://community.nxp.com/t5/S32K/Regarding-S32K142-Bootloader-using-PCAN/m-p/1632863#M22065</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;While browsing through NXP community, I found the following link for S32K142 Bootloader using PCAN.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have followed and downloaded the files provided which were ECU-BUS tool, and unified-bootloader-demo example codes.&lt;/P&gt;&lt;P&gt;Requirements:&lt;/P&gt;&lt;P&gt;1. I need to use PCAN to flash S32K142 board using normal CAN and not CAN-FD as I have hardware which supports only normal CAN.&lt;/P&gt;&lt;P&gt;Steps Followed:&lt;/P&gt;&lt;P&gt;1. As per the ECU-Guide provided in the above link has the details/settings mentioned which are for CAN-FD.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Importing the JSON file from the demo examples S32K142_CAN_user_config folder of&amp;nbsp;unified_bootloader_demo_v2.1 is based on CAN-FD.&lt;/P&gt;&lt;P&gt;Problems Faced.&lt;/P&gt;&lt;P&gt;1. The JSON file provided which should be imported for the UDS Services in ECU-BUS which is&amp;nbsp;ECUBUS_CANFD_uds.json is for CAN-FD normal CAN file is not provided.&lt;/P&gt;&lt;P&gt;Can you please provide me a JSON file for ECU-BUS and the normal CAN demo code which I can run and verify the bootloader using PCAN which supports only CAN and not CAN-FD. As I am only having the PCAN which supports CAN communication and not CAN-FD or LIN.&lt;/P&gt;</description>
    <pubDate>Mon, 17 Apr 2023 12:49:26 GMT</pubDate>
    <dc:creator>Dennis_Gokani</dc:creator>
    <dc:date>2023-04-17T12:49:26Z</dc:date>
    <item>
      <title>Regarding S32K142 Bootloader using PCAN</title>
      <link>https://community.nxp.com/t5/S32K/Regarding-S32K142-Bootloader-using-PCAN/m-p/1632863#M22065</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;While browsing through NXP community, I found the following link for S32K142 Bootloader using PCAN.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have followed and downloaded the files provided which were ECU-BUS tool, and unified-bootloader-demo example codes.&lt;/P&gt;&lt;P&gt;Requirements:&lt;/P&gt;&lt;P&gt;1. I need to use PCAN to flash S32K142 board using normal CAN and not CAN-FD as I have hardware which supports only normal CAN.&lt;/P&gt;&lt;P&gt;Steps Followed:&lt;/P&gt;&lt;P&gt;1. As per the ECU-Guide provided in the above link has the details/settings mentioned which are for CAN-FD.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Importing the JSON file from the demo examples S32K142_CAN_user_config folder of&amp;nbsp;unified_bootloader_demo_v2.1 is based on CAN-FD.&lt;/P&gt;&lt;P&gt;Problems Faced.&lt;/P&gt;&lt;P&gt;1. The JSON file provided which should be imported for the UDS Services in ECU-BUS which is&amp;nbsp;ECUBUS_CANFD_uds.json is for CAN-FD normal CAN file is not provided.&lt;/P&gt;&lt;P&gt;Can you please provide me a JSON file for ECU-BUS and the normal CAN demo code which I can run and verify the bootloader using PCAN which supports only CAN and not CAN-FD. As I am only having the PCAN which supports CAN communication and not CAN-FD or LIN.&lt;/P&gt;</description>
      <pubDate>Mon, 17 Apr 2023 12:49:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Regarding-S32K142-Bootloader-using-PCAN/m-p/1632863#M22065</guid>
      <dc:creator>Dennis_Gokani</dc:creator>
      <dc:date>2023-04-17T12:49:26Z</dc:date>
    </item>
  </channel>
</rss>