<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Pin details</title>
    <link>https://community.nxp.com/t5/S32K/Pin-details/m-p/1631549#M21999</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215430"&gt;@Divyashree1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The pin PTE13 for S32K342 is, by default, a GPIO which means that it is a digital input/output but can be configured as eMIOS_1_CH_H, LPSPI2_PCS2, LPSPI2_PCS0, FXIO_D5, EIRQ, VRC_CTRL or ADC1_S19.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB.&lt;/P&gt;</description>
    <pubDate>Tue, 11 Apr 2023 20:16:02 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2023-04-11T20:16:02Z</dc:date>
    <item>
      <title>Pin details</title>
      <link>https://community.nxp.com/t5/S32K/Pin-details/m-p/1631359#M21991</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;For Part number&amp;nbsp;S32K342NHT0MPBSR, Is the pin PTE13(11) Analog or Digital output pin?&lt;/P&gt;</description>
      <pubDate>Tue, 11 Apr 2023 12:51:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Pin-details/m-p/1631359#M21991</guid>
      <dc:creator>Divyashree1</dc:creator>
      <dc:date>2023-04-11T12:51:08Z</dc:date>
    </item>
    <item>
      <title>Re: Pin details</title>
      <link>https://community.nxp.com/t5/S32K/Pin-details/m-p/1631549#M21999</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215430"&gt;@Divyashree1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The pin PTE13 for S32K342 is, by default, a GPIO which means that it is a digital input/output but can be configured as eMIOS_1_CH_H, LPSPI2_PCS2, LPSPI2_PCS0, FXIO_D5, EIRQ, VRC_CTRL or ADC1_S19.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Apr 2023 20:16:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Pin-details/m-p/1631549#M21999</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-04-11T20:16:02Z</dc:date>
    </item>
  </channel>
</rss>