<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic s32k344 flexcan example in S32K</title>
    <link>https://community.nxp.com/t5/S32K/s32k344-flexcan-example/m-p/1631384#M21995</link>
    <description>&lt;P&gt;i want s32k344 flexcan code which run on normal/user mode&amp;nbsp;&lt;/P&gt;&lt;P&gt;i want to see output on bus like pcan or CANoe&lt;/P&gt;&lt;P&gt;if flex can is not available then classic can example for s32k3 series will be ok as of now i want to only test the pins of CAN&lt;/P&gt;</description>
    <pubDate>Tue, 11 Apr 2023 13:51:36 GMT</pubDate>
    <dc:creator>Jayraj1</dc:creator>
    <dc:date>2023-04-11T13:51:36Z</dc:date>
    <item>
      <title>s32k344 flexcan example</title>
      <link>https://community.nxp.com/t5/S32K/s32k344-flexcan-example/m-p/1631384#M21995</link>
      <description>&lt;P&gt;i want s32k344 flexcan code which run on normal/user mode&amp;nbsp;&lt;/P&gt;&lt;P&gt;i want to see output on bus like pcan or CANoe&lt;/P&gt;&lt;P&gt;if flex can is not available then classic can example for s32k3 series will be ok as of now i want to only test the pins of CAN&lt;/P&gt;</description>
      <pubDate>Tue, 11 Apr 2023 13:51:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k344-flexcan-example/m-p/1631384#M21995</guid>
      <dc:creator>Jayraj1</dc:creator>
      <dc:date>2023-04-11T13:51:36Z</dc:date>
    </item>
    <item>
      <title>Re: s32k344 flexcan example</title>
      <link>https://community.nxp.com/t5/S32K/s32k344-flexcan-example/m-p/1631692#M22006</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Jayraj1" target="_blank"&gt;Hi@Jayraj1&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;you can refer to this example ,post by Petr.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225" target="_self"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 03:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k344-flexcan-example/m-p/1631692#M22006</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-04-12T03:03:50Z</dc:date>
    </item>
  </channel>
</rss>