<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 MemoryAddress from Unified bootloader Demo</title>
    <link>https://community.nxp.com/t5/S32K/MemoryAddress-from-Unified-bootloader-Demo/m-p/1630736#M21957</link>
    <description>&lt;P&gt;Hello Nxp,&lt;/P&gt;&lt;P&gt;I'm integrating &lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099" target="_self"&gt;Unified bootloader Demo&lt;/A&gt; to my project so that I can flash S32K148 via CAN. I have some doubts about ECUBUS_CANFD_uds.json. For example,&amp;nbsp;flash_api.bin, how do we know that&amp;nbsp;"addressAndLengthFormatIdentifier" is "44" and&amp;nbsp;"memoryAddress" is "1FFFF800". The same for&amp;nbsp;S32K148_CAN_APP_Demo.bin, how to find that&amp;nbsp;"memoryAddress" is "0000F200"?&lt;/P&gt;&lt;P&gt;I'm asking because I have my own bin file, need to configure those values properly to flash.&lt;/P&gt;&lt;P&gt;Second question: when I use ECUBus tool to flash, after downloading&amp;nbsp;flash_api.bin successfully, the tool runs the routine 0x0202. 148 returns 0x78 means response is pending. How do I configure the tool to wait until 148 returns a positive response. With the current demo config, the tool fails without waiting for 148 to send the positive response.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;David&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 10 Apr 2023 21:37:33 GMT</pubDate>
    <dc:creator>DavidD1</dc:creator>
    <dc:date>2023-04-10T21:37:33Z</dc:date>
    <item>
      <title>MemoryAddress from Unified bootloader Demo</title>
      <link>https://community.nxp.com/t5/S32K/MemoryAddress-from-Unified-bootloader-Demo/m-p/1630736#M21957</link>
      <description>&lt;P&gt;Hello Nxp,&lt;/P&gt;&lt;P&gt;I'm integrating &lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099" target="_self"&gt;Unified bootloader Demo&lt;/A&gt; to my project so that I can flash S32K148 via CAN. I have some doubts about ECUBUS_CANFD_uds.json. For example,&amp;nbsp;flash_api.bin, how do we know that&amp;nbsp;"addressAndLengthFormatIdentifier" is "44" and&amp;nbsp;"memoryAddress" is "1FFFF800". The same for&amp;nbsp;S32K148_CAN_APP_Demo.bin, how to find that&amp;nbsp;"memoryAddress" is "0000F200"?&lt;/P&gt;&lt;P&gt;I'm asking because I have my own bin file, need to configure those values properly to flash.&lt;/P&gt;&lt;P&gt;Second question: when I use ECUBus tool to flash, after downloading&amp;nbsp;flash_api.bin successfully, the tool runs the routine 0x0202. 148 returns 0x78 means response is pending. How do I configure the tool to wait until 148 returns a positive response. With the current demo config, the tool fails without waiting for 148 to send the positive response.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;David&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Apr 2023 21:37:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MemoryAddress-from-Unified-bootloader-Demo/m-p/1630736#M21957</guid>
      <dc:creator>DavidD1</dc:creator>
      <dc:date>2023-04-10T21:37:33Z</dc:date>
    </item>
  </channel>
</rss>