<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Need Pin Clarification for Part number S32K342NHT0MPBSR in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Need-Pin-Clarification-for-Part-number-S32K342NHT0MPBSR/m-p/1629256#M21918</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;How the pin PTE13(11) output should be defined, Specifically the min and max output voltages. Also define the maximum current capability of this pin.&lt;/P&gt;</description>
    <pubDate>Thu, 06 Apr 2023 16:10:10 GMT</pubDate>
    <dc:creator>Divyashree1</dc:creator>
    <dc:date>2023-04-06T16:10:10Z</dc:date>
    <item>
      <title>Need Pin Clarification for Part number S32K342NHT0MPBSR</title>
      <link>https://community.nxp.com/t5/S32K/Need-Pin-Clarification-for-Part-number-S32K342NHT0MPBSR/m-p/1629256#M21918</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;How the pin PTE13(11) output should be defined, Specifically the min and max output voltages. Also define the maximum current capability of this pin.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Apr 2023 16:10:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-Pin-Clarification-for-Part-number-S32K342NHT0MPBSR/m-p/1629256#M21918</guid>
      <dc:creator>Divyashree1</dc:creator>
      <dc:date>2023-04-06T16:10:10Z</dc:date>
    </item>
    <item>
      <title>Re: Need Pin Clarification for Part number S32K342NHT0MPBSR</title>
      <link>https://community.nxp.com/t5/S32K/Need-Pin-Clarification-for-Part-number-S32K342NHT0MPBSR/m-p/1630387#M21943</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Divyashree1" target="_blank"&gt;Hi@Divyashree1&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;there is no Max output high current parameter.&lt;/P&gt;
&lt;P&gt;the output voltage should be euqal to VDD_HV_A and the Min output high current should be no less than 1.6 mA.&lt;/P&gt;
&lt;DIV id="tinyMceEditorSenlent_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_2-1681112716106.png" style="width: 642px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/218492i798134DD8DFA12EC/image-dimensions/642x285?v=v2" width="642" height="285" role="button" title="Senlent_2-1681112716106.png" alt="Senlent_2-1681112716106.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Apr 2023 07:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-Pin-Clarification-for-Part-number-S32K342NHT0MPBSR/m-p/1630387#M21943</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-04-10T07:49:11Z</dc:date>
    </item>
  </channel>
</rss>