<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can the channelB to N of ADC in S32K144 triggered by software? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Can-the-channelB-to-N-of-ADC-in-S32K144-triggered-by-software/m-p/762209#M2186</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You could also use SDK Peripheral Abstraction Layer (ADC PAL).&lt;/P&gt;&lt;P&gt;Which allows you to trigger a group of ADC conversions with a single SW or HW trigger.&lt;/P&gt;&lt;P&gt;SDK v0.8.5 includes adc_pal_example_s32k144&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="S32K144_ADC_PAL.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40641iEB3A3A065DB313CC/image-size/large?v=v2&amp;amp;px=999" role="button" title="S32K144_ADC_PAL.png" alt="S32K144_ADC_PAL.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 04 Feb 2018 22:51:03 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-02-04T22:51:03Z</dc:date>
    <item>
      <title>Can the channelB to N of ADC in S32K144 triggered by software?</title>
      <link>https://community.nxp.com/t5/S32K/Can-the-channelB-to-N-of-ADC-in-S32K144-triggered-by-software/m-p/762207#M2184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can't change the channel ID of the ADC using swtrigger to complete the conversion.&lt;span class="lia-inline-image-display-wrapper" image-alt="捕获.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30032iA3EC3E03AC737648/image-size/large?v=v2&amp;amp;px=999" role="button" title="捕获.PNG" alt="捕获.PNG" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The number of the channel can only be 0,i &amp;nbsp;can't get the result of conversion if i change it.&lt;/P&gt;&lt;P&gt;In the RM,i find this sentence: &lt;SPAN class=""&gt;None of the SC1B-SC1&lt;/SPAN&gt;&lt;SPAN class=""&gt;n &lt;/SPAN&gt;&lt;SPAN class=""&gt;registers are used for&lt;BR /&gt;software trigger operation and therefore writes to the SC1BSC1&lt;/SPAN&gt;&lt;SPAN class=""&gt;n &lt;/SPAN&gt;&lt;SPAN class=""&gt;registers do not initiate&lt;BR /&gt;a new conversion.&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;So,should i have to enable the pdb to&amp;nbsp;use multiple channels for AD conversion at the same time？&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope to get a reply as soon as possible.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jan 2018 13:10:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-the-channelB-to-N-of-ADC-in-S32K144-triggered-by-software/m-p/762207#M2184</guid>
      <dc:creator>timwang</dc:creator>
      <dc:date>2018-01-26T13:10:53Z</dc:date>
    </item>
    <item>
      <title>Re: Can the channelB to N of ADC in S32K144 triggered by software?</title>
      <link>https://community.nxp.com/t5/S32K/Can-the-channelB-to-N-of-ADC-in-S32K144-triggered-by-software/m-p/762208#M2185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I’m sorry for the late response.&lt;BR /&gt;Yes, only SCIA (SC1[chanIndex == 0]) can be used for software trigger.&lt;BR /&gt;And you can trigger only a single channel with a write to SCIA.&lt;BR /&gt;If you want to trigger more channels in a back-to-back conversion, use PDB.&lt;/P&gt;&lt;P&gt;You may refer to:&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-339644"&gt;https://community.nxp.com/docs/DOC-339644&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Feb 2018 14:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-the-channelB-to-N-of-ADC-in-S32K144-triggered-by-software/m-p/762208#M2185</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-02-02T14:24:49Z</dc:date>
    </item>
    <item>
      <title>Re: Can the channelB to N of ADC in S32K144 triggered by software?</title>
      <link>https://community.nxp.com/t5/S32K/Can-the-channelB-to-N-of-ADC-in-S32K144-triggered-by-software/m-p/762209#M2186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You could also use SDK Peripheral Abstraction Layer (ADC PAL).&lt;/P&gt;&lt;P&gt;Which allows you to trigger a group of ADC conversions with a single SW or HW trigger.&lt;/P&gt;&lt;P&gt;SDK v0.8.5 includes adc_pal_example_s32k144&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="S32K144_ADC_PAL.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40641iEB3A3A065DB313CC/image-size/large?v=v2&amp;amp;px=999" role="button" title="S32K144_ADC_PAL.png" alt="S32K144_ADC_PAL.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Feb 2018 22:51:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-the-channelB-to-N-of-ADC-in-S32K144-triggered-by-software/m-p/762209#M2186</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-02-04T22:51:03Z</dc:date>
    </item>
  </channel>
</rss>