<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: how Ecc works in S32k31x? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/how-Ecc-works-in-S32k31x/m-p/1624168#M21730</link>
    <description>&lt;P&gt;It is more complex. ECC is calculated generated from the polynomial, it is not simple sum.&lt;/P&gt;
&lt;P&gt;During checking it is not needed to recalculate and compare as according polynomial it can be checked directly.&lt;/P&gt;
&lt;P&gt;But it is unimportant for users, so it is not openly documented.&lt;/P&gt;</description>
    <pubDate>Wed, 29 Mar 2023 11:16:09 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2023-03-29T11:16:09Z</dc:date>
    <item>
      <title>how Ecc works in S32k31x?</title>
      <link>https://community.nxp.com/t5/S32K/how-Ecc-works-in-S32k31x/m-p/1622554#M21653</link>
      <description>&lt;P&gt;hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i want to know about Ecc.&lt;/P&gt;&lt;P&gt;In reference manual,&amp;nbsp;&lt;/P&gt;&lt;P&gt;The ECC is calculated over the sum of memory data and memory location address. However only data is written in the memory along with the ECC(address is excluded).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="hagoo_0-1679914829818.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/216398iDA076B42580A62B4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="hagoo_0-1679914829818.png" alt="hagoo_0-1679914829818.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is that mean, if memory = 3, and address = 0x00000001&lt;/P&gt;&lt;P&gt;1. write interface&lt;/P&gt;&lt;P&gt;- write 3(data) in 0x00000001(address)&lt;/P&gt;&lt;P&gt;- compute Ecc_1 ( data + address = 0x00000004)&lt;/P&gt;&lt;P&gt;2. Read interface&lt;/P&gt;&lt;P&gt;- recompute Ecc_2 ( Read data + address of Read data = 0x00000004)&lt;/P&gt;&lt;P&gt;- compare Ecc_1 and Ecc_2&lt;/P&gt;&lt;P&gt;- if (Ecc_1 != Ecc_2)&lt;/P&gt;&lt;P&gt;&amp;nbsp; Then Ecc Error occured!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I understand like this, it is right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 11:08:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/how-Ecc-works-in-S32k31x/m-p/1622554#M21653</guid>
      <dc:creator>hagoo</dc:creator>
      <dc:date>2023-03-27T11:08:54Z</dc:date>
    </item>
    <item>
      <title>Re: how Ecc works in S32k31x?</title>
      <link>https://community.nxp.com/t5/S32K/how-Ecc-works-in-S32k31x/m-p/1624168#M21730</link>
      <description>&lt;P&gt;It is more complex. ECC is calculated generated from the polynomial, it is not simple sum.&lt;/P&gt;
&lt;P&gt;During checking it is not needed to recalculate and compare as according polynomial it can be checked directly.&lt;/P&gt;
&lt;P&gt;But it is unimportant for users, so it is not openly documented.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Mar 2023 11:16:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/how-Ecc-works-in-S32k31x/m-p/1624168#M21730</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-03-29T11:16:09Z</dc:date>
    </item>
  </channel>
</rss>