<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to use S32K's FTM to generate variable-frequency square waves in S32K</title>
    <link>https://community.nxp.com/t5/S32K/How-to-use-S32K-s-FTM-to-generate-variable-frequency-square/m-p/760190#M2162</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.What mode is the channel configured into?&lt;/P&gt;&lt;P&gt;output compare or pwm?&lt;/P&gt;&lt;P&gt;2.Can give me an example for that?（The development environment is S32DS）&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Jun 2018 07:13:56 GMT</pubDate>
    <dc:creator>海斌蔡</dc:creator>
    <dc:date>2018-06-07T07:13:56Z</dc:date>
    <item>
      <title>How to use S32K's FTM to generate variable-frequency square waves</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-S32K-s-FTM-to-generate-variable-frequency-square/m-p/760190#M2162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.What mode is the channel configured into?&lt;/P&gt;&lt;P&gt;output compare or pwm?&lt;/P&gt;&lt;P&gt;2.Can give me an example for that?（The development environment is S32DS）&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 07:13:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-S32K-s-FTM-to-generate-variable-frequency-square/m-p/760190#M2162</guid>
      <dc:creator>海斌蔡</dc:creator>
      <dc:date>2018-06-07T07:13:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to use S32K's FTM to generate variable-frequency square waves</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-S32K-s-FTM-to-generate-variable-frequency-square/m-p/760191#M2163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;You can use both.&lt;BR /&gt;OC can clear, set or toggle the corresponding output pin on match. &lt;BR /&gt;PWM can be configured in different modes depending on your application requirements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN5303.pdf"&gt;AN5303 Features and Operation Modes of FlexTimer Module on S32K&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note-software/AN5303SW.zip"&gt;AN5303SW.zip&lt;/A&gt;&amp;nbsp;- please be aware that the project was built for the first 0N77P S32K144 maskset so the header files are outdated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 11:35:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-S32K-s-FTM-to-generate-variable-frequency-square/m-p/760191#M2163</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-06-07T11:35:55Z</dc:date>
    </item>
  </channel>
</rss>