<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K ECC RAM Initial</title>
    <link>https://community.nxp.com/t5/S32K/S32K-ECC-RAM-Initial/m-p/1621923#M21601</link>
    <description>&lt;P&gt;I have noted that there is an ECC RAM initial in the startup file of S32K116. (startup_S32K116.S)&lt;/P&gt;&lt;P&gt;I think this is related to AN12522.&lt;/P&gt;&lt;P&gt;My problem, it seems the&amp;nbsp;initialization only applied&amp;nbsp;SRAM_U. (0x2000_0000 to 0x2000_3800)&lt;/P&gt;&lt;P&gt;Is it no necessary to initial&amp;nbsp;SRAM_L because it is not ECC protected?&lt;/P&gt;</description>
    <pubDate>Sat, 25 Mar 2023 00:19:26 GMT</pubDate>
    <dc:creator>Ragus</dc:creator>
    <dc:date>2023-03-25T00:19:26Z</dc:date>
    <item>
      <title>S32K ECC RAM Initial</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ECC-RAM-Initial/m-p/1621923#M21601</link>
      <description>&lt;P&gt;I have noted that there is an ECC RAM initial in the startup file of S32K116. (startup_S32K116.S)&lt;/P&gt;&lt;P&gt;I think this is related to AN12522.&lt;/P&gt;&lt;P&gt;My problem, it seems the&amp;nbsp;initialization only applied&amp;nbsp;SRAM_U. (0x2000_0000 to 0x2000_3800)&lt;/P&gt;&lt;P&gt;Is it no necessary to initial&amp;nbsp;SRAM_L because it is not ECC protected?&lt;/P&gt;</description>
      <pubDate>Sat, 25 Mar 2023 00:19:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ECC-RAM-Initial/m-p/1621923#M21601</guid>
      <dc:creator>Ragus</dc:creator>
      <dc:date>2023-03-25T00:19:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K ECC RAM Initial</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ECC-RAM-Initial/m-p/1622103#M21615</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Ragus,&lt;/P&gt;
&lt;P&gt;Yes, your understanding is correct. Only the ECC-protected SRAM needs to be initialized.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AN12522.png" style="width: 905px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/216267iE319BE925B7721DF/image-size/large?v=v2&amp;amp;px=999" role="button" title="AN12522.png" alt="AN12522.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;AN12522.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 01:12:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ECC-RAM-Initial/m-p/1622103#M21615</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-03-27T01:12:43Z</dc:date>
    </item>
  </channel>
</rss>