<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K314 SPI flash implementation</title>
    <link>https://community.nxp.com/t5/S32K/S32K314-SPI-flash-implementation/m-p/1617504#M21457</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;I tried with this halfduplex format. But still it is having some error.&lt;BR /&gt;In mex file do I need to enable "SpiDeviceHalfDuplexSupport" option. In that there is another option SpiHalfDuplexPinSelect, in that if I select SOUT pin will it be act as both input and output.&lt;BR /&gt;Do you have any sample project of implementing LpSpi half duplex.&lt;/P&gt;</description>
    <pubDate>Fri, 17 Mar 2023 09:08:44 GMT</pubDate>
    <dc:creator>abhijith_r</dc:creator>
    <dc:date>2023-03-17T09:08:44Z</dc:date>
    <item>
      <title>S32K314 SPI flash implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-SPI-flash-implementation/m-p/1616922#M21432</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to implement SPI flash with S32K314 and using LpSpi. In that there is one function "Lpspi_Ip_SyncTransmit" which I assumes to write and read data. In this function a parameter length is there which is showing the length of data to be sent. In its definition the length is assigned to both tx and rx buffer. What to do if I am writing 1 byte of data and expecting more than 1 byte to receive.&lt;/P&gt;&lt;P&gt;In the spi flash data sheet an instruction 1 byte and expecting 3 bytes of data. We checked with logic analyzer, in that after transfering 1 byte clock is low.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone have a sample project of reading from SPI flash? Please share&lt;/P&gt;</description>
      <pubDate>Thu, 16 Mar 2023 14:34:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-SPI-flash-implementation/m-p/1616922#M21432</guid>
      <dc:creator>abhijith_r</dc:creator>
      <dc:date>2023-03-16T14:34:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 SPI flash implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-SPI-flash-implementation/m-p/1616961#M21434</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210364"&gt;@abhijith_r&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;What is the transfer format expected by the flash chip?&lt;/P&gt;
&lt;P&gt;The LPSPI can send 4 bytes in one transfer if the flash can ignore the 3 bytes at MOSI.&lt;/P&gt;
&lt;P&gt;Or the HalfDuplex APIs can be used instead.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1678981320126.png" style="width: 780px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/215044i6F7FD3A15EEFDE3F/image-dimensions/780x133?v=v2" width="780" height="133" role="button" title="danielmartynek_0-1678981320126.png" alt="danielmartynek_0-1678981320126.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1678981320126.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Depending on the Transfer type, the LPSPI module can either send data on the MOSI line or just receive data on the MISO line.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_1-1678981408905.png" style="width: 506px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/215045i6736D9EB210DB5E7/image-dimensions/506x120?v=v2" width="506" height="120" role="button" title="danielmartynek_1-1678981408905.png" alt="danielmartynek_1-1678981408905.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_1-1678981408905.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 16 Mar 2023 15:49:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-SPI-flash-implementation/m-p/1616961#M21434</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-03-16T15:49:10Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 SPI flash implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-SPI-flash-implementation/m-p/1617504#M21457</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;I tried with this halfduplex format. But still it is having some error.&lt;BR /&gt;In mex file do I need to enable "SpiDeviceHalfDuplexSupport" option. In that there is another option SpiHalfDuplexPinSelect, in that if I select SOUT pin will it be act as both input and output.&lt;BR /&gt;Do you have any sample project of implementing LpSpi half duplex.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Mar 2023 09:08:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-SPI-flash-implementation/m-p/1617504#M21457</guid>
      <dc:creator>abhijith_r</dc:creator>
      <dc:date>2023-03-17T09:08:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 SPI flash implementation</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-SPI-flash-implementation/m-p/1618490#M21501</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210364"&gt;@abhijith_r&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You can use the full-duplex mode too, if you fill the rest of the buffer with the IDLE data like (0xFF).&lt;/P&gt;
&lt;P&gt;Regarding the half duplex APIs, they can be used even when the module is not configured for a bidirectional single line SPI.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1679321797140.png" style="width: 511px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/215377iB4060ACD109E2187/image-dimensions/511x404?v=v2" width="511" height="404" role="button" title="danielmartynek_0-1679321797140.png" alt="danielmartynek_0-1679321797140.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1679321797140.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;My test code is attached.&lt;/P&gt;
&lt;P&gt;It sends 1 frame at MOSI and receives 3 frames at MISO using the half-duplex APIs.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 20 Mar 2023 14:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-SPI-flash-implementation/m-p/1618490#M21501</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-03-20T14:21:10Z</dc:date>
    </item>
  </channel>
</rss>