<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: UART uint8_t transmitter function [s32k144]</title>
    <link>https://community.nxp.com/t5/S32K/UART-uint8-t-transmitter-function-s32k144/m-p/757581#M2139</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;I was using Putty and it doesn't simulate it correctly, so i know that i wasn't using the right program, as always, Thanks Daniel!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Apr 2018 13:45:07 GMT</pubDate>
    <dc:creator>electronica2pow</dc:creator>
    <dc:date>2018-04-25T13:45:07Z</dc:date>
    <item>
      <title>UART uint8_t transmitter function [s32k144]</title>
      <link>https://community.nxp.com/t5/S32K/UART-uint8-t-transmitter-function-s32k144/m-p/757579#M2137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi to the community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to send an uint8_t number using this function:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void LPUART1_transmit_int(uint8_t number){&lt;BR /&gt; while((LPUART1-&amp;gt;STAT &amp;amp; LPUART_STAT_TDRE_MASK)&amp;gt;&amp;gt;LPUART_STAT_TDRE_SHIFT==0);&lt;BR /&gt; /* Wait for transmit buffer to be empty */&lt;BR /&gt; LPUART1-&amp;gt;DATA=number; /* Send data */&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But it doesn't work. I am going to attach the code below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The original one is:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void LPUART1_transmit_char(char send) { /* Function to Transmit single Char */&lt;BR /&gt; while((LPUART1-&amp;gt;STAT &amp;amp; LPUART_STAT_TDRE_MASK)&amp;gt;&amp;gt;LPUART_STAT_TDRE_SHIFT==0);&lt;BR /&gt; /* Wait for transmit buffer to be empty */&lt;BR /&gt; LPUART1-&amp;gt;DATA=send; /* Send data */&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Apr 2018 11:28:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/UART-uint8-t-transmitter-function-s32k144/m-p/757579#M2137</guid>
      <dc:creator>electronica2pow</dc:creator>
      <dc:date>2018-04-23T11:28:51Z</dc:date>
    </item>
    <item>
      <title>Re: UART uint8_t transmitter function [s32k144]</title>
      <link>https://community.nxp.com/t5/S32K/UART-uint8-t-transmitter-function-s32k144/m-p/757580#M2138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;If the program receives ‘1‘ in ascii which is 49, it will&amp;nbsp;return ‘&amp;gt;‘ (62) and uint8_t = 12.&lt;/P&gt;&lt;P&gt;It seems it works.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54010i4372FEDA537ED6EE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Apr 2018 15:35:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/UART-uint8-t-transmitter-function-s32k144/m-p/757580#M2138</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-04-24T15:35:49Z</dc:date>
    </item>
    <item>
      <title>Re: UART uint8_t transmitter function [s32k144]</title>
      <link>https://community.nxp.com/t5/S32K/UART-uint8-t-transmitter-function-s32k144/m-p/757581#M2139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;I was using Putty and it doesn't simulate it correctly, so i know that i wasn't using the right program, as always, Thanks Daniel!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2018 13:45:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/UART-uint8-t-transmitter-function-s32k144/m-p/757581#M2139</guid>
      <dc:creator>electronica2pow</dc:creator>
      <dc:date>2018-04-25T13:45:07Z</dc:date>
    </item>
  </channel>
</rss>