<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ethernet in MII mode in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Ethernet-in-MII-mode/m-p/1614035#M21315</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;yes, S32K148 support MII mode.&lt;BR /&gt;On MCU side, the ENET module have to be set for MII mode and all needed pins properly initialized.&lt;BR /&gt;Thy PHY must be set for MII mode as well, either using bootstrapping options or later by updating PHY registers using SMI interface.&lt;BR /&gt;&lt;SPAN&gt;TX_CLK/RX_CLK are inputs on MCU side, a PHY is generating those clock&amp;nbsp;&lt;/SPAN&gt;signals.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 13 Mar 2023 11:50:55 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-03-13T11:50:55Z</dc:date>
    <item>
      <title>Ethernet in MII mode</title>
      <link>https://community.nxp.com/t5/S32K/Ethernet-in-MII-mode/m-p/1613448#M21295</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using S32K148 Microcontroller, will it support MII mode with PHY?&lt;/P&gt;&lt;P&gt;What are settings needs to be done to work in MII&amp;nbsp;mode?&lt;/P&gt;&lt;P&gt;Should TX_CLK and RX_CLK configured for 2.5MHz/25MHz?&lt;/P&gt;</description>
      <pubDate>Sat, 11 Mar 2023 15:53:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Ethernet-in-MII-mode/m-p/1613448#M21295</guid>
      <dc:creator>rak14</dc:creator>
      <dc:date>2023-03-11T15:53:23Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet in MII mode</title>
      <link>https://community.nxp.com/t5/S32K/Ethernet-in-MII-mode/m-p/1614035#M21315</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;yes, S32K148 support MII mode.&lt;BR /&gt;On MCU side, the ENET module have to be set for MII mode and all needed pins properly initialized.&lt;BR /&gt;Thy PHY must be set for MII mode as well, either using bootstrapping options or later by updating PHY registers using SMI interface.&lt;BR /&gt;&lt;SPAN&gt;TX_CLK/RX_CLK are inputs on MCU side, a PHY is generating those clock&amp;nbsp;&lt;/SPAN&gt;signals.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Mar 2023 11:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Ethernet-in-MII-mode/m-p/1614035#M21315</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-03-13T11:50:55Z</dc:date>
    </item>
  </channel>
</rss>