<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K144 LIN Slave Diagnostics</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-LIN-Slave-Diagnostics/m-p/1613681#M21305</link>
    <description>&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;Thanks for your comments.&lt;/P&gt;&lt;P&gt;I will try your suggestions.&lt;/P&gt;</description>
    <pubDate>Mon, 13 Mar 2023 04:49:36 GMT</pubDate>
    <dc:creator>Punit_01</dc:creator>
    <dc:date>2023-03-13T04:49:36Z</dc:date>
    <item>
      <title>S32K144 LIN Slave Diagnostics</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-LIN-Slave-Diagnostics/m-p/1610600#M21177</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to implement LIN slave in S32K144 where it should support normal unconditional frames as well as Diagnostics with Class 2/3. (basically SID $10,$22,$2E are my minimum requirements).&lt;/P&gt;&lt;P&gt;Upon selecting the configuration in S32DS CT I have a bunch of files generated but i am finding it hard to understand the code structure.I have selected the LIN mode as slave &amp;amp; class 3. Additionally, i have selected "Support Diagnostics" &amp;amp; also selected the $2E service support.&lt;/P&gt;&lt;P&gt;When i browse the generated files &amp;amp; SDK, i see that there are some functions that are only applicable for a LIN Master.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It would be great if anyone can help me with some pointers on how to understand the generated files (may be some documentation?) &amp;amp; the callbacks which can be used to achieve the results.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the S32K144_SDK v4.0.1 with S32Ds v3.5.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 06:37:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-LIN-Slave-Diagnostics/m-p/1610600#M21177</guid>
      <dc:creator>Punit_01</dc:creator>
      <dc:date>2023-03-07T06:37:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 LIN Slave Diagnostics</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-LIN-Slave-Diagnostics/m-p/1610844#M21186</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213711"&gt;@Punit_01&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Regarding UDS, you can refer to this example.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K-SDK-LIN-Stack-not-working-properly-with-UDS/m-p/1313360" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K-SDK-LIN-Stack-not-working-properly-with-UDS/m-p/1313360&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Even though it was built with in S32DS 2.2. with older SDK (Processor Expert), it should be very similar.&lt;BR /&gt;&lt;BR /&gt;I believe the file structure is explained in the User Manual of the LIN Stack.&lt;BR /&gt;It is in the installation directory of the Stack.&lt;BR /&gt;Or it can be open from the CT (right-click on the lin stack component and select Documentation).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 10:54:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-LIN-Slave-Diagnostics/m-p/1610844#M21186</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-03-07T10:54:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 LIN Slave Diagnostics</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-LIN-Slave-Diagnostics/m-p/1613681#M21305</link>
      <description>&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;Thanks for your comments.&lt;/P&gt;&lt;P&gt;I will try your suggestions.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Mar 2023 04:49:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-LIN-Slave-Diagnostics/m-p/1613681#M21305</guid>
      <dc:creator>Punit_01</dc:creator>
      <dc:date>2023-03-13T04:49:36Z</dc:date>
    </item>
  </channel>
</rss>