<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K314 RTC code</title>
    <link>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1610595#M21176</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188029"&gt;@Senlent&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using S32K314 eval board. I added that code and in one example project and its working fine. In RTC IPL configuration, under GPTChannelConfigSet there is one option 'Rtc Channel Clock Source', it is set as "&lt;STRONG&gt;RTC_IP_CLOCK_SOURCE_2&lt;/STRONG&gt;" in that example project.&lt;/P&gt;&lt;P&gt;But when I try to implement this in our project there is only one option "&lt;STRONG&gt;RTC_IP_CLOCK_SOURCE_0&lt;/STRONG&gt;" and timer is not working properly. I can't change that to 2 via mex file.&lt;/P&gt;&lt;P&gt;But I manually edit&amp;nbsp; that value and change to&amp;nbsp;&lt;STRONG&gt;RTC_IP_CLOCK_SOURCE_2&amp;nbsp;&lt;/STRONG&gt;but when I call get time it is showing some wrong value (like clock is running very fastly). Later I change it to&amp;nbsp;&lt;STRONG&gt;RTC_IP_CLOCK_SOURCE_1&lt;/STRONG&gt;&amp;nbsp; and its working fine.&amp;nbsp; Why these options are not showing in mex file. How can I&amp;nbsp; change this option through mex file.&lt;/P&gt;</description>
    <pubDate>Tue, 07 Mar 2023 06:32:03 GMT</pubDate>
    <dc:creator>abhijith_r</dc:creator>
    <dc:date>2023-03-07T06:32:03Z</dc:date>
    <item>
      <title>S32K314 RTC code</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1608920#M21092</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working on s32k314, currently trying to implement RTC. But in example projects it is not found. Does anyone have an example project of RTC implementation?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Abhijith Raj&lt;/P&gt;</description>
      <pubDate>Fri, 03 Mar 2023 05:49:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1608920#M21092</guid>
      <dc:creator>abhijith_r</dc:creator>
      <dc:date>2023-03-03T05:49:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 RTC code</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1608971#M21096</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@abhijith_r" target="_blank"&gt;Hi@abhijith_r&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I sent you a private message, please check your message box.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Mar 2023 07:08:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1608971#M21096</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-03-03T07:08:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 RTC code</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1609000#M21098</link>
      <description>Hi Senlent,&lt;BR /&gt;Thanks for the quick reply. I got your message.</description>
      <pubDate>Fri, 03 Mar 2023 07:33:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1609000#M21098</guid>
      <dc:creator>abhijith_r</dc:creator>
      <dc:date>2023-03-03T07:33:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 RTC code</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1610595#M21176</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188029"&gt;@Senlent&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using S32K314 eval board. I added that code and in one example project and its working fine. In RTC IPL configuration, under GPTChannelConfigSet there is one option 'Rtc Channel Clock Source', it is set as "&lt;STRONG&gt;RTC_IP_CLOCK_SOURCE_2&lt;/STRONG&gt;" in that example project.&lt;/P&gt;&lt;P&gt;But when I try to implement this in our project there is only one option "&lt;STRONG&gt;RTC_IP_CLOCK_SOURCE_0&lt;/STRONG&gt;" and timer is not working properly. I can't change that to 2 via mex file.&lt;/P&gt;&lt;P&gt;But I manually edit&amp;nbsp; that value and change to&amp;nbsp;&lt;STRONG&gt;RTC_IP_CLOCK_SOURCE_2&amp;nbsp;&lt;/STRONG&gt;but when I call get time it is showing some wrong value (like clock is running very fastly). Later I change it to&amp;nbsp;&lt;STRONG&gt;RTC_IP_CLOCK_SOURCE_1&lt;/STRONG&gt;&amp;nbsp; and its working fine.&amp;nbsp; Why these options are not showing in mex file. How can I&amp;nbsp; change this option through mex file.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 06:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1610595#M21176</guid>
      <dc:creator>abhijith_r</dc:creator>
      <dc:date>2023-03-07T06:32:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 RTC code</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1611253#M21203</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@abhijith_r" target="_blank"&gt;Hi@abhijith_r&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Here you can modify the RTC Clock Source,then you can change "RTC_IP_CLOCK_SOURCE_X"&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1678240215047.png" style="width: 482px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/213612iB06E3A9F40686164/image-dimensions/482x267?v=v2" width="482" height="267" role="button" title="Senlent_0-1678240215047.png" alt="Senlent_0-1678240215047.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_0-1678240215047.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Mar 2023 01:54:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1611253#M21203</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-03-08T01:54:10Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 RTC code</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1864938#M35309</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210364"&gt;@abhijith_r&lt;/a&gt;&amp;nbsp; ,yes your correct . in API there is no option to change clock source its default clock 0 only, RTC is working in Clock source 1.&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 05:14:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-RTC-code/m-p/1864938#M35309</guid>
      <dc:creator>Prasanth_C</dc:creator>
      <dc:date>2024-05-14T05:14:47Z</dc:date>
    </item>
  </channel>
</rss>