<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What circumstances will cause the adc self-test algorithm return failure in S32K3xx in S32K</title>
    <link>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1610570#M21174</link>
    <description>&lt;P&gt;I am testing the ADC Self Test function on the S32K324 chip.&lt;/P&gt;&lt;P&gt;In order to test that the ADC can be detected when an error occurs, the ADC Reference high voltage is artificially set to zero on the hardware circuit to simulate ADC failure, but the ADC Self-Test algorithm still does not report an error (I use the AUTOSAR standard interface selftest API)&lt;/P&gt;&lt;P&gt;I confirmed that I removed the corresponding circuit because the ADC calibration did not pass and will enter dead loop.&lt;/P&gt;&lt;P&gt;I wonder what will cause the self test function failed and how I can test it.&lt;/P&gt;&lt;P&gt;B.R.&lt;/P&gt;&lt;P&gt;Guo&lt;/P&gt;</description>
    <pubDate>Tue, 07 Mar 2023 05:44:26 GMT</pubDate>
    <dc:creator>Guo-</dc:creator>
    <dc:date>2023-03-07T05:44:26Z</dc:date>
    <item>
      <title>What circumstances will cause the adc self-test algorithm return failure in S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1610570#M21174</link>
      <description>&lt;P&gt;I am testing the ADC Self Test function on the S32K324 chip.&lt;/P&gt;&lt;P&gt;In order to test that the ADC can be detected when an error occurs, the ADC Reference high voltage is artificially set to zero on the hardware circuit to simulate ADC failure, but the ADC Self-Test algorithm still does not report an error (I use the AUTOSAR standard interface selftest API)&lt;/P&gt;&lt;P&gt;I confirmed that I removed the corresponding circuit because the ADC calibration did not pass and will enter dead loop.&lt;/P&gt;&lt;P&gt;I wonder what will cause the self test function failed and how I can test it.&lt;/P&gt;&lt;P&gt;B.R.&lt;/P&gt;&lt;P&gt;Guo&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 05:44:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1610570#M21174</guid>
      <dc:creator>Guo-</dc:creator>
      <dc:date>2023-03-07T05:44:26Z</dc:date>
    </item>
    <item>
      <title>Re: What circumstances will cause the adc self-test algorithm return failure in S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1610890#M21193</link>
      <description>&lt;P&gt;I don't understand you whether you are setting VREFH to low during self-test or only during calibration. Anyway ADC self-test algorithm S tests reference voltage, so it should lead failed self-test results.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 12:24:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1610890#M21193</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-03-07T12:24:16Z</dc:date>
    </item>
    <item>
      <title>Re: What circumstances will cause the adc self-test algorithm return failure in S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1611367#M21208</link>
      <description>&lt;P&gt;I removed the &lt;SPAN&gt;VREFH circuit&amp;nbsp;&lt;/SPAN&gt;on the physical circuit. That means there is no input at this pin. Wheather&amp;nbsp;that the&amp;nbsp;&lt;SPAN&gt;VREFH &lt;/SPAN&gt;needs to be grounded to make the self test error?&amp;nbsp;I just simply disconnected &lt;SPAN&gt;VREFH pin. At the following image, I would like to show you how I start the self test after set the adc register to the correct value, and I hope it is helpful for you to find out why the self-test didn't work.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Mar 2023 05:19:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1611367#M21208</guid>
      <dc:creator>Guo-</dc:creator>
      <dc:date>2023-03-08T05:19:13Z</dc:date>
    </item>
    <item>
      <title>Re: What circumstances will cause the adc self-test algorithm return failure in S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1611766#M21228</link>
      <description>&lt;P&gt;It is quite interesting, but it is possible that if you have VREFH unconnected, it may be evaluated as valid range due to induced voltage from other pins (not being completely sure). I would recommend you to try to terminate to GND.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Mar 2023 16:26:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1611766#M21228</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-03-08T16:26:34Z</dc:date>
    </item>
    <item>
      <title>Re: What circumstances will cause the adc self-test algorithm return failure in S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1612042#M21242</link>
      <description>&lt;P&gt;Nope it still not work&lt;/P&gt;&lt;P&gt;I ground VREFH as you asked but self-test API still returns pass&lt;/P&gt;&lt;P&gt;To make the problem clearer, I would like to confirm to you whether I changed the circuit correctly: I ground the 16th pin of the MCU chip, other circuits do not change, I am using the S32K324 chip (S32K324&amp;nbsp; has 172 pins)&lt;/P&gt;&lt;P&gt;I would also like to know which error register would set 1 under “normal” circumstances?&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;ADC_STSR1_ERR_S0 or&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;ADC_STSR1_ERR_S1 or&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;ADC_STSR1_ERR_S2?&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 09 Mar 2023 05:15:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1612042#M21242</guid>
      <dc:creator>Guo-</dc:creator>
      <dc:date>2023-03-09T05:15:20Z</dc:date>
    </item>
    <item>
      <title>Re: What circumstances will cause the adc self-test algorithm return failure in S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1612442#M21258</link>
      <description>&lt;P&gt;I should fail is S0 as it converts band gap level according ADC reference.&lt;/P&gt;</description>
      <pubDate>Thu, 09 Mar 2023 13:25:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1612442#M21258</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-03-09T13:25:08Z</dc:date>
    </item>
    <item>
      <title>Re: What circumstances will cause the adc self-test algorithm return failure in S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1612780#M21271</link>
      <description>&lt;P&gt;I still don't understand why self-test didn't work. After I turned on all the registers related to self-test as required by the chip reference manual, I could observe the repeated changes from 0 to 1 in the SELF_TEST_S (18bit) from MSR register by leaving the register in this state, which proves that selftest has started normally.&lt;/P&gt;&lt;P&gt;But the STSR1 register only has bit23 turned to 1(value: 0x00800000) which confirmed self-test end of conversion, I don't know after normal selftest ends, only bit23 in STSR1 will set 1 or the watch dog register should set to complete.&lt;/P&gt;&lt;P&gt;But according to your statement, bit11 in the STSR1 register, the Error Algorithm S step 0, will be set to 1 first?&lt;/P&gt;&lt;P&gt;I still need your help with this problem,I would like you to give me some ideas, or should I provide more clues?&lt;/P&gt;</description>
      <pubDate>Fri, 10 Mar 2023 02:28:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1612780#M21271</guid>
      <dc:creator>Guo-</dc:creator>
      <dc:date>2023-03-10T02:28:35Z</dc:date>
    </item>
    <item>
      <title>Re: What circumstances will cause the adc self-test algorithm return failure in S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1615632#M21392</link>
      <description>&lt;P&gt;I have obtained an answer from SW developer, I am forwarding as it is:&lt;/P&gt;
&lt;P&gt;"&lt;/P&gt;
&lt;P&gt;The reason for the self-test executed successfully with VREFH tied to GND is that, the RTD Adc_Sar_Ip_SelfTest() only executes the self-test process but doesn't check the conversion data of each self-test algorithm step(such as S1), it means the error flag(such as STSR1[ERR_S1]) won't be set although the VREFH was tied to GND.&lt;/P&gt;
&lt;P&gt;And the ADC also provides monitoring options for conversion data generated by self-test algorithms, for details, you could refer to "58.3.16.2.4 Self-test analog watchdog" in S32K3 RM.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.png" style="width: 689px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/214679iBF6E9E208D21ED57/image-dimensions/689x574?v=v2" width="689" height="574" role="button" title="1.png" alt="1.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;To help the customer to complete this test, we need to enable the self-test analog watchdog and configure its low threshold value(15bit) which related to VERFH(self-test algorithm S1 and S2).&lt;/P&gt;
&lt;P&gt;For example, I modified the RTD Adc_Sar_Ip_SelfTest() function by adding below code, then the self-test was failed because the conversion data(0x7DE0) of S1|S2 was less than the low threshold value which I configured(0x7FFF) before.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="2.png" style="width: 714px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/214680iA163F14474380DE0/image-dimensions/714x227?v=v2" width="714" height="227" role="button" title="2.png" alt="2.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;2.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You could also find the conversion result when an error in step 1|2 of algorithm S has occurred as below.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="3.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/214681iD3C514E69FC5C6BD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="3.png" alt="3.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;3.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;
&lt;P&gt; &lt;/P&gt;
&lt;P&gt; &lt;/P&gt;
&lt;P&gt;"&lt;/P&gt;</description>
      <pubDate>Wed, 15 Mar 2023 10:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1615632#M21392</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-03-15T10:23:33Z</dc:date>
    </item>
    <item>
      <title>Re: What circumstances will cause the adc self-test algorithm return failure in S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1617205#M21441</link>
      <description>&lt;P&gt;So in fact, in the autosar framework, the selftest api cannot detect whether the adc circuit outside the chip is working properly, but only whether the adc is working properly inside the chip. I think I got it. Thanks a lot.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Mar 2023 01:30:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1617205#M21441</guid>
      <dc:creator>Guo-</dc:creator>
      <dc:date>2023-03-17T01:30:51Z</dc:date>
    </item>
    <item>
      <title>Re: What circumstances will cause the adc self-test algorithm return failure in S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1746513#M28166</link>
      <description>hi, are these code written by you manually, or from S32K Design Studio with some package?</description>
      <pubDate>Thu, 26 Oct 2023 02:58:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-circumstances-will-cause-the-adc-self-test-algorithm-return/m-p/1746513#M28166</guid>
      <dc:creator>LeoZ</dc:creator>
      <dc:date>2023-10-26T02:58:38Z</dc:date>
    </item>
  </channel>
</rss>