<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: unresolved inclusion in S32K</title>
    <link>https://community.nxp.com/t5/S32K/unresolved-inclusion/m-p/1608795#M21088</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;What IDE are you using? S32 Design Studio for ARM Version 2.2 ?&lt;BR /&gt;Did you select S32K1 SDK when creating project? Refer to this article: &lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-the-Blinking-LED-example-project-using-S32K144-SDK/ta-p/1128260" target="_self"&gt;HOWTO: Create the Blinking LED example project using S32K144 SDK&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
    <pubDate>Fri, 03 Mar 2023 01:25:42 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2023-03-03T01:25:42Z</dc:date>
    <item>
      <title>unresolved inclusion</title>
      <link>https://community.nxp.com/t5/S32K/unresolved-inclusion/m-p/1607311#M21022</link>
      <description>&lt;P&gt;When I try to include the source header files in the main function, the system reports an error of unresolved inclusion. The osurce files are from the debug section of the project explorer.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="screenshot.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/212791i176A430D201473B7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="screenshot.png" alt="screenshot.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;screenshot.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Wed, 01 Mar 2023 04:00:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/unresolved-inclusion/m-p/1607311#M21022</guid>
      <dc:creator>JackHuangZeyu</dc:creator>
      <dc:date>2023-03-01T04:00:39Z</dc:date>
    </item>
    <item>
      <title>Re: unresolved inclusion</title>
      <link>https://community.nxp.com/t5/S32K/unresolved-inclusion/m-p/1608795#M21088</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;What IDE are you using? S32 Design Studio for ARM Version 2.2 ?&lt;BR /&gt;Did you select S32K1 SDK when creating project? Refer to this article: &lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-the-Blinking-LED-example-project-using-S32K144-SDK/ta-p/1128260" target="_self"&gt;HOWTO: Create the Blinking LED example project using S32K144 SDK&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
      <pubDate>Fri, 03 Mar 2023 01:25:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/unresolved-inclusion/m-p/1608795#M21088</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-03-03T01:25:42Z</dc:date>
    </item>
  </channel>
</rss>