<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SPI problem when changing to a higher frequency in S32K</title>
    <link>https://community.nxp.com/t5/S32K/SPI-problem-when-changing-to-a-higher-frequency/m-p/750305#M2081</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running SPI at 1MHz speed on EVB board with a polling method similar to the one on S32DS example, but for continuous transmission of 256 bytes. When I change the speed to 10MHz some data bytes I receive at my beagle are distorted (if I was sending 0x55 for all bytes, I received a different value on some of them), seem to be the SPI lines are quite noise. Is there a hardware change that need to be done for higher frequencies or is the the EVB capable of handling that frequency?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Feb 2018 16:06:40 GMT</pubDate>
    <dc:creator>emmanuelaguilas</dc:creator>
    <dc:date>2018-02-15T16:06:40Z</dc:date>
    <item>
      <title>SPI problem when changing to a higher frequency</title>
      <link>https://community.nxp.com/t5/S32K/SPI-problem-when-changing-to-a-higher-frequency/m-p/750305#M2081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running SPI at 1MHz speed on EVB board with a polling method similar to the one on S32DS example, but for continuous transmission of 256 bytes. When I change the speed to 10MHz some data bytes I receive at my beagle are distorted (if I was sending 0x55 for all bytes, I received a different value on some of them), seem to be the SPI lines are quite noise. Is there a hardware change that need to be done for higher frequencies or is the the EVB capable of handling that frequency?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Feb 2018 16:06:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPI-problem-when-changing-to-a-higher-frequency/m-p/750305#M2081</guid>
      <dc:creator>emmanuelaguilas</dc:creator>
      <dc:date>2018-02-15T16:06:40Z</dc:date>
    </item>
    <item>
      <title>Re: SPI problem when changing to a higher frequency</title>
      <link>https://community.nxp.com/t5/S32K/SPI-problem-when-changing-to-a-higher-frequency/m-p/750306#M2082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;The MCU supports 10MHz SPI baud rate which is the fastest rate in Run Mode without the loopback option (Table 31 of the S32Kxx Data sheet).&lt;BR /&gt;Please note that the measurements were taken with fastest slew setting PORT_PCRn[DSE = 1] (Table 12, 13 of the DS).&lt;BR /&gt;So please use high-drive pins, labeled as GPIO-HD in S32K144_IO_Signal_Description_Input_Multiplexing.xlsx&lt;BR /&gt;Regarding EVB, I don’t see any problem with that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Feb 2018 22:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPI-problem-when-changing-to-a-higher-frequency/m-p/750306#M2082</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-02-15T22:03:04Z</dc:date>
    </item>
  </channel>
</rss>