<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックDisable eMIOS from input pin via TRGMUX</title>
    <link>https://community.nxp.com/t5/S32K/Disable-eMIOS-from-input-pin-via-TRGMUX/m-p/1601139#M20748</link>
    <description>&lt;P&gt;Hi, I am trying to disable eMIOS channels from an input pin using the MCAL.&lt;BR /&gt;I am using S32K312 with RTD 2.0.0 D2203.&lt;/P&gt;&lt;P&gt;In the Port config the input pin is set to TRGMUX_TRGMUX_IN6 and in Trgmux Logic Group the hardware input is set to TRGMUX_IP_INPUT_SIUL2_IN6 and hardware output to TGMUX_IP_OUTPUT_EMIOS012_ODIS0. So far, so good I think.&lt;/P&gt;&lt;P&gt;Then in Pwm/ Emios Instance the Output Disable Source is greyed out and I cannot find how to activate the setting.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="oskarjohansson_0-1676638520920.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/211391i94232364EA0A447A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="oskarjohansson_0-1676638520920.png" alt="oskarjohansson_0-1676638520920.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Oskar&lt;/P&gt;</description>
    <pubDate>Fri, 17 Feb 2023 12:56:34 GMT</pubDate>
    <dc:creator>oskarjohansson</dc:creator>
    <dc:date>2023-02-17T12:56:34Z</dc:date>
    <item>
      <title>Disable eMIOS from input pin via TRGMUX</title>
      <link>https://community.nxp.com/t5/S32K/Disable-eMIOS-from-input-pin-via-TRGMUX/m-p/1601139#M20748</link>
      <description>&lt;P&gt;Hi, I am trying to disable eMIOS channels from an input pin using the MCAL.&lt;BR /&gt;I am using S32K312 with RTD 2.0.0 D2203.&lt;/P&gt;&lt;P&gt;In the Port config the input pin is set to TRGMUX_TRGMUX_IN6 and in Trgmux Logic Group the hardware input is set to TRGMUX_IP_INPUT_SIUL2_IN6 and hardware output to TGMUX_IP_OUTPUT_EMIOS012_ODIS0. So far, so good I think.&lt;/P&gt;&lt;P&gt;Then in Pwm/ Emios Instance the Output Disable Source is greyed out and I cannot find how to activate the setting.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="oskarjohansson_0-1676638520920.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/211391i94232364EA0A447A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="oskarjohansson_0-1676638520920.png" alt="oskarjohansson_0-1676638520920.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Oskar&lt;/P&gt;</description>
      <pubDate>Fri, 17 Feb 2023 12:56:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Disable-eMIOS-from-input-pin-via-TRGMUX/m-p/1601139#M20748</guid>
      <dc:creator>oskarjohansson</dc:creator>
      <dc:date>2023-02-17T12:56:34Z</dc:date>
    </item>
    <item>
      <title>Re: Disable eMIOS from input pin via TRGMUX</title>
      <link>https://community.nxp.com/t5/S32K/Disable-eMIOS-from-input-pin-via-TRGMUX/m-p/1601857#M20763</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@oskarjohansson" target="_blank"&gt;Hi@oskarjohansson&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I spent some time researching, and it's the same on my side, and I can't find a place to configure it.&lt;/P&gt;
&lt;P&gt;I need to communicate with the IDE team to confirm whether this is a bug,&lt;/P&gt;
&lt;P&gt;At present, you can modify it manually,&lt;/P&gt;
&lt;P&gt;thanks for your report.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Feb 2023 09:50:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Disable-eMIOS-from-input-pin-via-TRGMUX/m-p/1601857#M20763</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-02-20T09:50:38Z</dc:date>
    </item>
    <item>
      <title>Re: Disable eMIOS from input pin via TRGMUX</title>
      <link>https://community.nxp.com/t5/S32K/Disable-eMIOS-from-input-pin-via-TRGMUX/m-p/1602033#M20773</link>
      <description>&lt;P&gt;Okay! I will do that meanwhile.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Oskar&lt;/P&gt;</description>
      <pubDate>Mon, 20 Feb 2023 13:31:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Disable-eMIOS-from-input-pin-via-TRGMUX/m-p/1602033#M20773</guid>
      <dc:creator>oskarjohansson</dc:creator>
      <dc:date>2023-02-20T13:31:20Z</dc:date>
    </item>
  </channel>
</rss>