<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: About Time Quanta and SSP offset</title>
    <link>https://community.nxp.com/t5/S32K/About-Time-Quanta-and-SSP-offset/m-p/620475#M207</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;The bit time during an Arbitration phase is defined by CTRL1 or CBT register.&lt;/P&gt;&lt;P&gt;Note the CBT must be used when CAN FD feature is enabled.&lt;/P&gt;&lt;P&gt;Then the length of bit can have below time quantas.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15948iDBA03EFCDBBA835F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The bit time for the Data phase is defined by FDCBT register, as below, if the bit rate switching is enabled for CAN FD frame (FDCTRL[FDRATE]=1 and the BRS bit of the Tx MBs is set). Otherwise CTRL1 or CBT registers control bit time of Data phase.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15987i537C44698C07ACB3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;The position of the secondary sample point is defined by the measured loop delay time added to an offset value specified in CAN_FDCTRL[TDCOFF]. CAN_FDCTRL[TDCVAL] bit field stores the result of this calculation.&lt;/P&gt;&lt;P&gt;The TDC mechanism can be enabled by the CAN_FDCTRL[TDCEN] bit and is effectiveonly during the data phase of FD frames having the BRS bit set. It has no effect either on non-FD frames, or on FD frames transmitted at normal bit rate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Mar 2017 06:26:36 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2017-03-29T06:26:36Z</dc:date>
    <item>
      <title>About Time Quanta and SSP offset</title>
      <link>https://community.nxp.com/t5/S32K/About-Time-Quanta-and-SSP-offset/m-p/620474#M206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I have been developping CAN FD related item.&lt;/P&gt;&lt;P&gt;And I have to check Time Quanta and SSP(secondary sample point) offset.&lt;/P&gt;&lt;P&gt;So please someone helps me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;Time Quanta&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; - at CAN FD frame, Time Quanta in Arbitration phase and Data phase are 5 ~ 48 TQ range. right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;captured on page 1293&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17649iAEB2D9723D051E4C/image-size/large?v=v2&amp;amp;px=999" title="제목 없음.png" alt="제목 없음.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. How to&amp;nbsp;check SSP offset value?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;- at debuging window, there is not any value.&lt;/P&gt;&lt;P&gt;&amp;lt;captured on S32DS debuging window&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17697iE3C035FAB35F8B7C/image-size/large?v=v2&amp;amp;px=999" title="제목 없음1.jpg" alt="제목 없음1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Kim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Mar 2017 10:10:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-Time-Quanta-and-SSP-offset/m-p/620474#M206</guid>
      <dc:creator>kimjunghyun</dc:creator>
      <dc:date>2017-03-27T10:10:05Z</dc:date>
    </item>
    <item>
      <title>Re: About Time Quanta and SSP offset</title>
      <link>https://community.nxp.com/t5/S32K/About-Time-Quanta-and-SSP-offset/m-p/620475#M207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;The bit time during an Arbitration phase is defined by CTRL1 or CBT register.&lt;/P&gt;&lt;P&gt;Note the CBT must be used when CAN FD feature is enabled.&lt;/P&gt;&lt;P&gt;Then the length of bit can have below time quantas.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15948iDBA03EFCDBBA835F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The bit time for the Data phase is defined by FDCBT register, as below, if the bit rate switching is enabled for CAN FD frame (FDCTRL[FDRATE]=1 and the BRS bit of the Tx MBs is set). Otherwise CTRL1 or CBT registers control bit time of Data phase.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15987i537C44698C07ACB3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;The position of the secondary sample point is defined by the measured loop delay time added to an offset value specified in CAN_FDCTRL[TDCOFF]. CAN_FDCTRL[TDCVAL] bit field stores the result of this calculation.&lt;/P&gt;&lt;P&gt;The TDC mechanism can be enabled by the CAN_FDCTRL[TDCEN] bit and is effectiveonly during the data phase of FD frames having the BRS bit set. It has no effect either on non-FD frames, or on FD frames transmitted at normal bit rate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Mar 2017 06:26:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-Time-Quanta-and-SSP-offset/m-p/620475#M207</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-03-29T06:26:36Z</dc:date>
    </item>
    <item>
      <title>Re: About Time Quanta and SSP offset</title>
      <link>https://community.nxp.com/t5/S32K/About-Time-Quanta-and-SSP-offset/m-p/620476#M208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. Petr.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For question 1, Time quanta, I understood as below.&lt;/P&gt;&lt;P&gt;&amp;nbsp;- CAN FD arbitration phase : using CAN_CBT&lt;/P&gt;&lt;P&gt;&amp;nbsp;- CAN FD data phase : using CAN_FDCBT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For question 2, How to&amp;nbsp;check SSP offset value, I understood your explanation.&lt;/P&gt;&lt;P&gt;But I could not&amp;nbsp;confirm that &amp;nbsp;the&amp;nbsp;bit of TDCEN and TDCOFF was changed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;- I changed the&amp;nbsp;bit of TDCEN and TDCOFF at the EmbSys Registers but these bits were not changed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;- So I&amp;nbsp;changed these&amp;nbsp;bits at the source code, but I&amp;nbsp;was not sure that these bits were changed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Because&amp;nbsp;these bits&amp;nbsp;at the EmbSys Registers&amp;nbsp;were changed(1) during RUN but&amp;nbsp;were returned to initial value(0) during SUSPEND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;How can I change&amp;nbsp;the bit&amp;nbsp;of TDCEN and TDCOFF and confirm whether changed or not?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Should&amp;nbsp;I think these bit as changed?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;■ At the EmbSys Registers&amp;nbsp;:&lt;/P&gt;&lt;P&gt;&amp;nbsp;1. I changed TDCEN bit to 1&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9227i865B44F221F777DA/image-size/large?v=v2&amp;amp;px=999" title="TDCEN.jpg" alt="TDCEN.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;2. but this bit was not changed (the bit was returned to initial value 0, TDC is disabled)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8939i740EC986DF742110/image-size/large?v=v2&amp;amp;px=999" title="TDCEN_변경안됨.jpg" alt="TDCEN_변경안됨.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;■ At the source code :&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;1. I changed TDCEN bit to 1&lt;/P&gt;&lt;P&gt;&amp;lt; Before code change &amp;gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9357i7C05FBB3A9310EC0/image-size/large?v=v2&amp;amp;px=999" title="TDCEN_code.jpg" alt="TDCEN_code.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;lt; After code change : from x to 1 &amp;gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9692i86FAD56B2E43D428/image-size/large?v=v2&amp;amp;px=999" title="TDCEN_code_변경.jpg" alt="TDCEN_code_변경.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;2. and&amp;nbsp;TDCEN bit&amp;nbsp;was&amp;nbsp;changed&amp;nbsp;(enabled) during&amp;nbsp;RUN.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9812iA59062328B888A50/image-size/large?v=v2&amp;amp;px=999" title="TDCEN_code_변경_반영됨.jpg" alt="TDCEN_code_변경_반영됨.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;3. but TDCEN bit&amp;nbsp;was returned to initial value&amp;nbsp;(disabled) during SUSPEND&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9650i8C87F21BB8D3129E/image-size/large?v=v2&amp;amp;px=999" title="TDCEN_code_변경_반영안됨.jpg" alt="TDCEN_code_변경_반영안됨.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Kim.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Apr 2017 06:58:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-Time-Quanta-and-SSP-offset/m-p/620476#M208</guid>
      <dc:creator>kimjunghyun</dc:creator>
      <dc:date>2017-04-19T06:58:59Z</dc:date>
    </item>
  </channel>
</rss>