<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックInterrupts only serviced on core0</title>
    <link>https://community.nxp.com/t5/S32K/Interrupts-only-serviced-on-core0/m-p/1597512#M20598</link>
    <description>&lt;P&gt;I would like an interrupt to be generated at the end of conversion of the ADC but I am only able to see these interrupts being serviced on core0 on my s32k322.&lt;/P&gt;&lt;P&gt;I have set the Target core for the ADC instance I am working with to core 1 (unchecked M7_0 and checked M7_1) in the Config Tool. If I enable core0 as target for these interrupts, the interrupts get triggered as expected, calling the ISR.&lt;/P&gt;&lt;P&gt;Is there any additional setting/mode required to allow servicing of ISRs on the cores other than core0? I am also unable to see the configuration being written to the IRSPRC registers as they all show up as "- not read -" as shown in the attached screenshot.&lt;/P&gt;</description>
    <pubDate>Fri, 10 Feb 2023 17:27:13 GMT</pubDate>
    <dc:creator>winsmen</dc:creator>
    <dc:date>2023-02-10T17:27:13Z</dc:date>
    <item>
      <title>Interrupts only serviced on core0</title>
      <link>https://community.nxp.com/t5/S32K/Interrupts-only-serviced-on-core0/m-p/1597512#M20598</link>
      <description>&lt;P&gt;I would like an interrupt to be generated at the end of conversion of the ADC but I am only able to see these interrupts being serviced on core0 on my s32k322.&lt;/P&gt;&lt;P&gt;I have set the Target core for the ADC instance I am working with to core 1 (unchecked M7_0 and checked M7_1) in the Config Tool. If I enable core0 as target for these interrupts, the interrupts get triggered as expected, calling the ISR.&lt;/P&gt;&lt;P&gt;Is there any additional setting/mode required to allow servicing of ISRs on the cores other than core0? I am also unable to see the configuration being written to the IRSPRC registers as they all show up as "- not read -" as shown in the attached screenshot.&lt;/P&gt;</description>
      <pubDate>Fri, 10 Feb 2023 17:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Interrupts-only-serviced-on-core0/m-p/1597512#M20598</guid>
      <dc:creator>winsmen</dc:creator>
      <dc:date>2023-02-10T17:27:13Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupts only serviced on core0</title>
      <link>https://community.nxp.com/t5/S32K/Interrupts-only-serviced-on-core0/m-p/1598166#M20644</link>
      <description>&lt;P&gt;Hi, could you share your project?&lt;/P&gt;</description>
      <pubDate>Mon, 13 Feb 2023 12:02:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Interrupts-only-serviced-on-core0/m-p/1598166#M20644</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-02-13T12:02:07Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupts only serviced on core0</title>
      <link>https://community.nxp.com/t5/S32K/Interrupts-only-serviced-on-core0/m-p/1598255#M20649</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52613"&gt;@davidtosenovjan&lt;/a&gt;! I am unable to share my entire project publicly, but I'd be happy to share relevant snippets that could assist you in helping me figure this out.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Feb 2023 14:55:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Interrupts-only-serviced-on-core0/m-p/1598255#M20649</guid>
      <dc:creator>winsmen</dc:creator>
      <dc:date>2023-02-13T14:55:27Z</dc:date>
    </item>
  </channel>
</rss>