<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: About KITFS85SKTEVM pin configuration when programming with S32K144 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/About-KITFS85SKTEVM-pin-configuration-when-programming-with/m-p/1597511#M20597</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Once again, thank you for using the NXP community.&lt;/P&gt;
&lt;P&gt;Note that an external LDO is provided to feed VDDI2C. This LDO can also be used to feed VDDIO, which is the default implementation. The LDO is supplied by 5.0 V coming from the USB.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diazmarin09_0-1676049932435.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210519iB615FD94898BF3FC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="diazmarin09_0-1676049932435.png" alt="diazmarin09_0-1676049932435.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you will supply your the board using the USB, I do recommend using the default configuration (3.3V) as VDDIO is the input voltage of the SPI module.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
    <pubDate>Fri, 10 Feb 2023 17:25:48 GMT</pubDate>
    <dc:creator>diazmarin09</dc:creator>
    <dc:date>2023-02-10T17:25:48Z</dc:date>
    <item>
      <title>About KITFS85SKTEVM pin configuration when programming with S32K144</title>
      <link>https://community.nxp.com/t5/S32K/About-KITFS85SKTEVM-pin-configuration-when-programming-with/m-p/1596672#M20551</link>
      <description>&lt;P&gt;Hello everyone&lt;/P&gt;&lt;P&gt;I read that if the user wants to connect the SPI to another MCU, this is possible.I want to write it whether it should be connected to the VDDIO and VDDI2C pins on the j11 pin. I want to communicate with SPI.&lt;/P&gt;&lt;P&gt;Thanks..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 14:58:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-KITFS85SKTEVM-pin-configuration-when-programming-with/m-p/1596672#M20551</guid>
      <dc:creator>yavuzklc</dc:creator>
      <dc:date>2023-02-09T14:58:08Z</dc:date>
    </item>
    <item>
      <title>Re: About KITFS85SKTEVM pin configuration when programming with S32K144</title>
      <link>https://community.nxp.com/t5/S32K/About-KITFS85SKTEVM-pin-configuration-when-programming-with/m-p/1596889#M20555</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I hope all is great with you. Thank you for using the NXP communities.&lt;/P&gt;
&lt;P&gt;You are correct, digital signals such as SPI are accessible through connectors.&lt;/P&gt;
&lt;P&gt;In this case, as the kit uses a KL25Z MCU to communicate with FlexGUI, you need to disconnect the KL25Z in order to connect your MCU.&lt;/P&gt;
&lt;P&gt;In this case, &lt;STRONG&gt;remove J28&lt;/STRONG&gt; and appropriate jumpers to &lt;STRONG&gt;disconnect&lt;/STRONG&gt; the KL25Z MCU (see Figure 5) and &lt;STRONG&gt;connect&lt;/STRONG&gt; the external MCU on J30 connector as shown in Figure 6. In addition to this change, &lt;U&gt;make sure that the VDDIO voltage domain is the same on MCU side and SBC side&lt;/U&gt;.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diazmarin09_0-1675983070440.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210371iC10B2C9B6A3E14C2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="diazmarin09_0-1675983070440.png" alt="diazmarin09_0-1675983070440.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diazmarin09_1-1675983073897.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210372iBDD55111FB43F30A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="diazmarin09_1-1675983073897.png" alt="diazmarin09_1-1675983073897.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this information helps.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 22:51:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-KITFS85SKTEVM-pin-configuration-when-programming-with/m-p/1596889#M20555</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-02-09T22:51:45Z</dc:date>
    </item>
    <item>
      <title>Re: About KITFS85SKTEVM pin configuration when programming with S32K144</title>
      <link>https://community.nxp.com/t5/S32K/About-KITFS85SKTEVM-pin-configuration-when-programming-with/m-p/1597059#M20559</link>
      <description>&lt;P&gt;In fact i want to ask thing about J11 port. Should the 5th and 6th pins remain connected or seperate (VDDIO and VDDI2C) while communicating with the other mcu spi?&lt;/P&gt;</description>
      <pubDate>Fri, 10 Feb 2023 06:20:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-KITFS85SKTEVM-pin-configuration-when-programming-with/m-p/1597059#M20559</guid>
      <dc:creator>yavuzklc</dc:creator>
      <dc:date>2023-02-10T06:20:50Z</dc:date>
    </item>
    <item>
      <title>Re: About KITFS85SKTEVM pin configuration when programming with S32K144</title>
      <link>https://community.nxp.com/t5/S32K/About-KITFS85SKTEVM-pin-configuration-when-programming-with/m-p/1597511#M20597</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Once again, thank you for using the NXP community.&lt;/P&gt;
&lt;P&gt;Note that an external LDO is provided to feed VDDI2C. This LDO can also be used to feed VDDIO, which is the default implementation. The LDO is supplied by 5.0 V coming from the USB.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diazmarin09_0-1676049932435.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210519iB615FD94898BF3FC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="diazmarin09_0-1676049932435.png" alt="diazmarin09_0-1676049932435.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you will supply your the board using the USB, I do recommend using the default configuration (3.3V) as VDDIO is the input voltage of the SPI module.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Fri, 10 Feb 2023 17:25:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/About-KITFS85SKTEVM-pin-configuration-when-programming-with/m-p/1597511#M20597</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-02-10T17:25:48Z</dc:date>
    </item>
  </channel>
</rss>