<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Preferred Compiler for S32K3</title>
    <link>https://community.nxp.com/t5/S32K/Preferred-Compiler-for-S32K3/m-p/1597443#M20592</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I'm not sure if you mean the compiler itself or the entire development IDE.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Anyway, S32DS offers plugins for all mentioned compilers.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I will leave the choice of preference to the user, it can be based on habit or experience, or other requirements.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;GCC is a free compiler.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;But in case your application requires to be ISO26262 compliant, it requires a certified compiler, as I know IAR, GHS and Diab are certified, but also they are not free.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There may be other differences, such as how effectively they are able to optimize code compilation and the like. Here I would refer to public resources.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 10 Feb 2023 15:33:06 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2023-02-10T15:33:06Z</dc:date>
    <item>
      <title>Preferred Compiler for S32K3</title>
      <link>https://community.nxp.com/t5/S32K/Preferred-Compiler-for-S32K3/m-p/1596479#M20541</link>
      <description>&lt;P&gt;Hi, i wanted to know, is there preferred compiler for the S32K3 uC? There are several choices, gcc, greenhill, IAR, when i take a look at the introduction of S32DS that it can interact with different compilers. But i ask myself, when using this uC, is there preferred compiler?&lt;/P&gt;&lt;P&gt;Tks.&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 09:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Preferred-Compiler-for-S32K3/m-p/1596479#M20541</guid>
      <dc:creator>YiGao</dc:creator>
      <dc:date>2023-02-09T09:57:58Z</dc:date>
    </item>
    <item>
      <title>Re: Preferred Compiler for S32K3</title>
      <link>https://community.nxp.com/t5/S32K/Preferred-Compiler-for-S32K3/m-p/1597443#M20592</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I'm not sure if you mean the compiler itself or the entire development IDE.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Anyway, S32DS offers plugins for all mentioned compilers.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I will leave the choice of preference to the user, it can be based on habit or experience, or other requirements.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;GCC is a free compiler.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;But in case your application requires to be ISO26262 compliant, it requires a certified compiler, as I know IAR, GHS and Diab are certified, but also they are not free.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There may be other differences, such as how effectively they are able to optimize code compilation and the like. Here I would refer to public resources.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Feb 2023 15:33:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Preferred-Compiler-for-S32K3/m-p/1597443#M20592</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-02-10T15:33:06Z</dc:date>
    </item>
  </channel>
</rss>