<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K344 eMIOS trigger BCTU ADC List in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-eMIOS-trigger-BCTU-ADC-List/m-p/1595544#M20508</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;can you share modified project to see whole setting and code used? So we can test it?&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Wed, 08 Feb 2023 11:23:11 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-02-08T11:23:11Z</dc:date>
    <item>
      <title>S32K344 eMIOS trigger BCTU ADC List</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-eMIOS-trigger-BCTU-ADC-List/m-p/1594695#M20485</link>
      <description>&lt;P&gt;I am using S32K344 with RTD 2.0.0 D2203 and trying to implement a PWM center triggered ADC list reading.&lt;/P&gt;&lt;P&gt;I have tested the example&amp;nbsp;when the BCTU is software triggered &lt;A href="https://community.nxp.com/t5/S32K/How-BCTU-LIST-items-works/m-p/1577227#M19813" target="_blank"&gt;https://community.nxp.com/t5/S32K/How-BCTU-LIST-items-works/m-p/1577227#M19813&lt;/A&gt;&amp;nbsp;and it seems to work good and I am able to configure the ADC channels I want to use.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then I am trying to add a eMIOS channel, for now eMIOS_0_0 in MCB_UP_DOWN_COUNTER in Emios_Mcl_Ip_1 and use it as the trigger source in BCTU, which is default from the example above.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="oskarjohansson_0-1675769969318.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209943i5880131A02DAA1AC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="oskarjohansson_0-1675769969318.png" alt="oskarjohansson_0-1675769969318.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But the BCTU is never triggered and it is not possible to software trigger the BCTU anymore.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;/P&gt;&lt;P&gt;Oskar Johansson&lt;/P&gt;</description>
      <pubDate>Tue, 07 Feb 2023 11:41:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-eMIOS-trigger-BCTU-ADC-List/m-p/1594695#M20485</guid>
      <dc:creator>oskarjohansson</dc:creator>
      <dc:date>2023-02-07T11:41:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 eMIOS trigger BCTU ADC List</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-eMIOS-trigger-BCTU-ADC-List/m-p/1595544#M20508</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;can you share modified project to see whole setting and code used? So we can test it?&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 08 Feb 2023 11:23:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-eMIOS-trigger-BCTU-ADC-List/m-p/1595544#M20508</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-02-08T11:23:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 eMIOS trigger BCTU ADC List</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-eMIOS-trigger-BCTU-ADC-List/m-p/1595782#M20520</link>
      <description>&lt;P&gt;Here is the whole project attached. I have tested it against the evaluation board:&amp;nbsp;&lt;SPAN&gt;S32K3X4EVB-Q257.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Oskar&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Feb 2023 17:06:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-eMIOS-trigger-BCTU-ADC-List/m-p/1595782#M20520</guid>
      <dc:creator>oskarjohansson</dc:creator>
      <dc:date>2023-02-08T17:06:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 eMIOS trigger BCTU ADC List</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-eMIOS-trigger-BCTU-ADC-List/m-p/1596471#M20540</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;have below option selected in the BCTU setting&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1675936252787.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210280i96E0E2725BF3DD0D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_0-1675936252787.png" alt="PetrS_0-1675936252787.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;It clears MCR[FRZ] bit within BCTU init so HW triggers will be enabled.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 09:52:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-eMIOS-trigger-BCTU-ADC-List/m-p/1596471#M20540</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-02-09T09:52:13Z</dc:date>
    </item>
  </channel>
</rss>