<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Memory overlap after adding some stuff to the linker</title>
    <link>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1593890#M20463</link>
    <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52613"&gt;@davidtosenovjan&lt;/a&gt;, thank you for reaching out.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Yea, at least 3 times as also I've tried some other stuff but I had no luck.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there anything else that I can provide you with in order to help you ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;kyf.&lt;/P&gt;</description>
    <pubDate>Mon, 06 Feb 2023 10:23:12 GMT</pubDate>
    <dc:creator>kyf</dc:creator>
    <dc:date>2023-02-06T10:23:12Z</dc:date>
    <item>
      <title>Memory overlap after adding some stuff to the linker</title>
      <link>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1592340#M20390</link>
      <description>&lt;P&gt;Hello NXP team.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm getting a memory overlap issue. The memory overlap is happening between the non_cacheable_data section and the itcm_code section that I've added into the linker.&lt;BR /&gt;&lt;BR /&gt;The error message that I'm getting is this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kyf_0-1675342394267.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209366i222B422971530E18/image-size/large?v=v2&amp;amp;px=999" alt="kyf_0-1675342394267.png" title="kyf_0-1675342394267.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've done the same changes into a newly SIUL2 project and I had no issues. When I've tried to apply the same changes into the linker + startup_cm7.s code into the project that I'm working on I've got the memory overlap issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working with S32K344 devboard RTD drivers 2.0. I've attached the linker and the startup code that I've used.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Am I missing something here ?&lt;/P&gt;&lt;P&gt;I've looked into the linker file and I could find no memory overlap addresses.&lt;/P&gt;&lt;P&gt;I need to copy my ISR into ITCM memory and run it from there but at the moment I've stuck with the memory overlap issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you need any extra info let me know.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;kyf&lt;/P&gt;</description>
      <pubDate>Thu, 02 Feb 2023 13:00:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1592340#M20390</guid>
      <dc:creator>kyf</dc:creator>
      <dc:date>2023-02-02T13:00:09Z</dc:date>
    </item>
    <item>
      <title>Re: Memory overlap after adding some stuff to the linker</title>
      <link>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1593843#M20459</link>
      <description>&lt;P&gt;I have checked you files and I haven't found anything obviously wrong. Have you tried to Clean Project and recompile?&lt;/P&gt;</description>
      <pubDate>Mon, 06 Feb 2023 09:30:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1593843#M20459</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-02-06T09:30:01Z</dc:date>
    </item>
    <item>
      <title>Re: Memory overlap after adding some stuff to the linker</title>
      <link>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1593890#M20463</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52613"&gt;@davidtosenovjan&lt;/a&gt;, thank you for reaching out.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Yea, at least 3 times as also I've tried some other stuff but I had no luck.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there anything else that I can provide you with in order to help you ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;kyf.&lt;/P&gt;</description>
      <pubDate>Mon, 06 Feb 2023 10:23:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1593890#M20463</guid>
      <dc:creator>kyf</dc:creator>
      <dc:date>2023-02-06T10:23:12Z</dc:date>
    </item>
    <item>
      <title>Re: Memory overlap after adding some stuff to the linker</title>
      <link>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1594843#M20492</link>
      <description>&lt;P&gt;I have tried to open new example based on Siul2_Port_Ip_Example_S32K344&lt;/P&gt;
&lt;P&gt;modifying linker command file and and startup file as you attached (adding all lines marked as additional, if I compare with originals) and I see no error after compiling.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Feb 2023 15:31:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1594843#M20492</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-02-07T15:31:52Z</dc:date>
    </item>
    <item>
      <title>Re: Memory overlap after adding some stuff to the linker</title>
      <link>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1596522#M20543</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52613"&gt;@davidtosenovjan&lt;/a&gt; .&lt;/P&gt;&lt;P&gt;I have done this also and I get no error in compiling. But with my project I get the compile error regarding the linker.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What do you believe can affect the generated files in that stage of the&amp;nbsp; build ? Does anything comes to mind ?&lt;BR /&gt;&lt;BR /&gt;I've double checked the memory regions used within the .ld file and I could not find anything missed there.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;kyf&lt;/P&gt;</description>
      <pubDate>Thu, 09 Feb 2023 10:58:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1596522#M20543</guid>
      <dc:creator>kyf</dc:creator>
      <dc:date>2023-02-09T10:58:36Z</dc:date>
    </item>
    <item>
      <title>Re: Memory overlap after adding some stuff to the linker</title>
      <link>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1597270#M20574</link>
      <description>&lt;P&gt;Unfortunately I have no idea.&lt;/P&gt;
&lt;P&gt;You could possibly share the whole project. If you don't want to do it on this public place I would recommend to enter a support ticket:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/support/support:SUPPORTHOME" target="_blank"&gt;https://www.nxp.com/support/support:SUPPORTHOME&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Feb 2023 10:45:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Memory-overlap-after-adding-some-stuff-to-the-linker/m-p/1597270#M20574</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-02-10T10:45:27Z</dc:date>
    </item>
  </channel>
</rss>