<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックDifferences of RTD develop package</title>
    <link>https://community.nxp.com/t5/S32K/Differences-of-RTD-develop-package/m-p/1592038#M20371</link>
    <description>&lt;P&gt;Hi Team&lt;/P&gt;&lt;P&gt;We would like to start a project on S32K342. However, we used S32K344 to test some demo. We now want to transfer S32K344 to S32K342. Some errors appear.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The RTD package we use before is "SW32K3_RTD_4.4_1.0.0_DS_updatesite_D2110", There is no S32K342. Then we changed it to "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204". When we build the project which is successful on S32K344 with "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204" on S32K342, there are a lot of errors. The name of some value changes and some API disappear.&lt;/P&gt;&lt;P&gt;What can I correct them? Or we can not build the project with 2.0.0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 02 Feb 2023 07:30:50 GMT</pubDate>
    <dc:creator>Hermit</dc:creator>
    <dc:date>2023-02-02T07:30:50Z</dc:date>
    <item>
      <title>Differences of RTD develop package</title>
      <link>https://community.nxp.com/t5/S32K/Differences-of-RTD-develop-package/m-p/1592038#M20371</link>
      <description>&lt;P&gt;Hi Team&lt;/P&gt;&lt;P&gt;We would like to start a project on S32K342. However, we used S32K344 to test some demo. We now want to transfer S32K344 to S32K342. Some errors appear.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The RTD package we use before is "SW32K3_RTD_4.4_1.0.0_DS_updatesite_D2110", There is no S32K342. Then we changed it to "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204". When we build the project which is successful on S32K344 with "SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204" on S32K342, there are a lot of errors. The name of some value changes and some API disappear.&lt;/P&gt;&lt;P&gt;What can I correct them? Or we can not build the project with 2.0.0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Feb 2023 07:30:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Differences-of-RTD-develop-package/m-p/1592038#M20371</guid>
      <dc:creator>Hermit</dc:creator>
      <dc:date>2023-02-02T07:30:50Z</dc:date>
    </item>
    <item>
      <title>Re: Differences of RTD develop package</title>
      <link>https://community.nxp.com/t5/S32K/Differences-of-RTD-develop-package/m-p/1592416#M20397</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Hermit,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;SW32K3_RTD_4.4_1.0.0_DS_updatesite_D2110 does not support S32K342, if you want to use S32K342 please install SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P style="font-weight: 400;"&gt;The difference between the S32K344 and S32K342 is not just the size of flash memory and RAM. Search for "S32K342" in S32K3XXRM to see all differences.&amp;nbsp;&lt;/P&gt;
&lt;P style="font-weight: 400;"&gt;Please create new project for S32K342 with RTD2.0.0, import the .mex file and copy the code manually.&amp;nbsp;&lt;/P&gt;
&lt;P style="font-weight: 400;"&gt;BTW, you can take a look at&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/Low-RTD-version-project-immigrating-to-higher-version/m-p/1446058#M8459" target="_self"&gt;Low RTD version project immigrating to higher version&lt;/A&gt;&lt;/P&gt;
&lt;P style="font-weight: 400;"&gt;Sorry for the inconvenience we bring you!&lt;/P&gt;
&lt;P style="font-weight: 400;"&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 02 Feb 2023 14:31:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Differences-of-RTD-develop-package/m-p/1592416#M20397</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-02-02T14:31:17Z</dc:date>
    </item>
    <item>
      <title>Re: Differences of RTD develop package</title>
      <link>https://community.nxp.com/t5/S32K/Differences-of-RTD-develop-package/m-p/1592703#M20404</link>
      <description>&lt;P&gt;HI Robin&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Hermit&lt;/P&gt;</description>
      <pubDate>Fri, 03 Feb 2023 01:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Differences-of-RTD-develop-package/m-p/1592703#M20404</guid>
      <dc:creator>Hermit</dc:creator>
      <dc:date>2023-02-03T01:23:42Z</dc:date>
    </item>
  </channel>
</rss>