<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How do I stop the LPIT counter from counting while jlink is debugging In S32K118 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/How-do-I-stop-the-LPIT-counter-from-counting-while-jlink-is/m-p/1591631#M20355</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/208982"&gt;@Xiao-xiao-pang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you help me confirmin if you are using the EVB? Also, which software and version are you using?&lt;/P&gt;</description>
    <pubDate>Wed, 01 Feb 2023 21:33:52 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2023-02-01T21:33:52Z</dc:date>
    <item>
      <title>How do I stop the LPIT counter from counting while jlink is debugging In S32K118</title>
      <link>https://community.nxp.com/t5/S32K/How-do-I-stop-the-LPIT-counter-from-counting-while-jlink-is/m-p/1591272#M20345</link>
      <description>&lt;P&gt;&lt;SPAN&gt;While I was debugging the code, the LPIT timer count was decreasing while the code was running.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;triggering the LPIT interrupt。&lt;/SPAN&gt;I don't expect the counter value of LPIT0 to change when in debug。How to set the register?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="4f08ae2d72aaab73ab09b733fffe9b2.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209125iB0ED52DE1138FB77/image-size/large?v=v2&amp;amp;px=999" role="button" title="4f08ae2d72aaab73ab09b733fffe9b2.png" alt="4f08ae2d72aaab73ab09b733fffe9b2.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;4f08ae2d72aaab73ab09b733fffe9b2.png&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Feb 2023 11:58:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-do-I-stop-the-LPIT-counter-from-counting-while-jlink-is/m-p/1591272#M20345</guid>
      <dc:creator>Xiao-xiao-pang</dc:creator>
      <dc:date>2023-02-01T11:58:51Z</dc:date>
    </item>
    <item>
      <title>Re: How do I stop the LPIT counter from counting while jlink is debugging In S32K118</title>
      <link>https://community.nxp.com/t5/S32K/How-do-I-stop-the-LPIT-counter-from-counting-while-jlink-is/m-p/1591631#M20355</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/208982"&gt;@Xiao-xiao-pang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you help me confirmin if you are using the EVB? Also, which software and version are you using?&lt;/P&gt;</description>
      <pubDate>Wed, 01 Feb 2023 21:33:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-do-I-stop-the-LPIT-counter-from-counting-while-jlink-is/m-p/1591631#M20355</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-02-01T21:33:52Z</dc:date>
    </item>
  </channel>
</rss>