<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Power Manager Component not appearing in Configuration Tools</title>
    <link>https://community.nxp.com/t5/S32K/Power-Manager-Component-not-appearing-in-Configuration-Tools/m-p/1588244#M20228</link>
    <description>&lt;P&gt;I have the exact same issue in S32 Designs Studio V3.5. But i don't want too switch to the ARM version, because as far as i can tell this is an older version. And the newer versions should be capable of the same, right? What can be the cause it's not showing in the configuration tools?&lt;/P&gt;</description>
    <pubDate>Thu, 26 Jan 2023 10:15:00 GMT</pubDate>
    <dc:creator>melvinw</dc:creator>
    <dc:date>2023-01-26T10:15:00Z</dc:date>
    <item>
      <title>Power Manager Component not appearing in Configuration Tools</title>
      <link>https://community.nxp.com/t5/S32K/Power-Manager-Component-not-appearing-in-Configuration-Tools/m-p/1567697#M19368</link>
      <description>&lt;P&gt;I am currently working on a project with an S32K144 MCU. I am also using a MC33742 SBC to provide the 5v supply.&lt;/P&gt;&lt;P&gt;For part of the application, I need to put the SBC into stop mode. In stop mode, the SBC can only provide 10-20mA, or it is woken up. In order to achieve this low-current requirement, I am trying to put the MCU into Very Low Power Run (VLPR) mode.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;To switch from normal run mode to VLPR, I have added the power_manager module from the S32K144 SDK. The problem I'm running into is that I can't see or add the power manager component in the configuration tool. Is there a step somewhere that I'm missing?&lt;/P&gt;</description>
      <pubDate>Fri, 09 Dec 2022 23:07:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-Manager-Component-not-appearing-in-Configuration-Tools/m-p/1567697#M19368</guid>
      <dc:creator>DCouture</dc:creator>
      <dc:date>2022-12-09T23:07:44Z</dc:date>
    </item>
    <item>
      <title>Re: Power Manager Component not appearing in Configuration Tools</title>
      <link>https://community.nxp.com/t5/S32K/Power-Manager-Component-not-appearing-in-Configuration-Tools/m-p/1567830#M19374</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@DCouture" target="_blank" rel="noopener"&gt;Hi@DCouture&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;please take a look at tthe demo in the S32 DS, I attached the picture for your reference.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1670811853055.png" style="width: 617px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/203868iB264E29E6F124E7C/image-dimensions/617x390?v=v2" width="617" height="390" role="button" title="Senlent_0-1670811853055.png" alt="Senlent_0-1670811853055.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_0-1670811853055.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR!&lt;/P&gt;</description>
      <pubDate>Mon, 12 Dec 2022 02:24:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-Manager-Component-not-appearing-in-Configuration-Tools/m-p/1567830#M19374</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2022-12-12T02:24:31Z</dc:date>
    </item>
    <item>
      <title>Re: Power Manager Component not appearing in Configuration Tools</title>
      <link>https://community.nxp.com/t5/S32K/Power-Manager-Component-not-appearing-in-Configuration-Tools/m-p/1568580#M19397</link>
      <description>&lt;P&gt;I think I have figured out my issue. I switched from using the S32DS for S32K v3.5 to S32DS for ARM v2.2. I can find the Power Manager now and interact with it.&lt;/P&gt;</description>
      <pubDate>Mon, 12 Dec 2022 21:37:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-Manager-Component-not-appearing-in-Configuration-Tools/m-p/1568580#M19397</guid>
      <dc:creator>DCouture</dc:creator>
      <dc:date>2022-12-12T21:37:09Z</dc:date>
    </item>
    <item>
      <title>Re: Power Manager Component not appearing in Configuration Tools</title>
      <link>https://community.nxp.com/t5/S32K/Power-Manager-Component-not-appearing-in-Configuration-Tools/m-p/1588244#M20228</link>
      <description>&lt;P&gt;I have the exact same issue in S32 Designs Studio V3.5. But i don't want too switch to the ARM version, because as far as i can tell this is an older version. And the newer versions should be capable of the same, right? What can be the cause it's not showing in the configuration tools?&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jan 2023 10:15:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Power-Manager-Component-not-appearing-in-Configuration-Tools/m-p/1588244#M20228</guid>
      <dc:creator>melvinw</dc:creator>
      <dc:date>2023-01-26T10:15:00Z</dc:date>
    </item>
  </channel>
</rss>