<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: FreeRTOS stuck in prvPortStartFirstTask</title>
    <link>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1586034#M20152</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have the same issue on the same example and I have FreeRTOS for S32K3 2.0.1.&lt;/P&gt;&lt;P&gt;Can someone explain what is the root cause of this?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Lucian&lt;/P&gt;</description>
    <pubDate>Fri, 20 Jan 2023 13:06:18 GMT</pubDate>
    <dc:creator>lucianmocanu_zzzzz</dc:creator>
    <dc:date>2023-01-20T13:06:18Z</dc:date>
    <item>
      <title>FreeRTOS stuck in prvPortStartFirstTask</title>
      <link>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1418594#M14121</link>
      <description>&lt;P&gt;I am running a project in which I use FreeRTOS and a few drivers. Nothing too fancy. I'm using the SEGEGR J-Link debugger, and I kept running into this problem at startup.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MateoSegura413_0-1645679534580.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171587i140C9BBBF5E81E53/image-size/medium?v=v2&amp;amp;px=400" role="button" title="MateoSegura413_0-1645679534580.png" alt="MateoSegura413_0-1645679534580.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I thought it was my code, so I decided to go ahead and use the blinky example provided by NXP. No modifications no nothing. Same error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone have any idea why this happens?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 23 Feb 2022 22:16:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1418594#M14121</guid>
      <dc:creator>MateoSegura413</dc:creator>
      <dc:date>2022-02-23T22:16:03Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS stuck in prvPortStartFirstTask</title>
      <link>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1419316#M14147</link>
      <description>&lt;P&gt;Hi Mateo,&lt;/P&gt;
&lt;P&gt;do you mean this example?&lt;/P&gt;
&lt;P&gt;c:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2021_10\FreeRTOS\examples\S32DS\FreeRTOS_Toggle_Led_Example_S32K344\&lt;/P&gt;
&lt;P&gt;I just tested this one on my board with Multilink FX and it works as expected on my side...&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 18:47:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1419316#M14147</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-02-24T18:47:10Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS stuck in prvPortStartFirstTask</title>
      <link>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1419325#M14149</link>
      <description>&lt;P&gt;Hello, yes it's that example. I tried to re install the FreeRTOS extension and it works correctly now. Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 19:12:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1419325#M14149</guid>
      <dc:creator>MateoSegura413</dc:creator>
      <dc:date>2022-02-24T19:12:15Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS stuck in prvPortStartFirstTask</title>
      <link>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1465826#M15704</link>
      <description>&lt;P&gt;Hi Mateo,&amp;nbsp;&lt;/P&gt;&lt;P&gt;What do you mean by "re installed the FreeRTOS extension"?&lt;/P&gt;&lt;P&gt;I'm&amp;nbsp;facing the same issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Adde&lt;/P&gt;</description>
      <pubDate>Sat, 28 May 2022 18:48:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1465826#M15704</guid>
      <dc:creator>adde_ado</dc:creator>
      <dc:date>2022-05-28T18:48:54Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS stuck in prvPortStartFirstTask</title>
      <link>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1466384#M15732</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184112"&gt;@adde_ado&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Update to version 2.0 of the drivers as well as FreeRTOS.&lt;/P&gt;&lt;P&gt;This will resolve all these problems.&lt;/P&gt;&lt;P&gt;Also, if you have a Jlink debugger, try downgrading to a lower version of the Jlink firmware.&lt;/P&gt;&lt;P&gt;In our experience, the PNE micro debugger has always worked with no issues, but we've run into quite a few issues with JLink. Most dev kits will have a PNE micro debugger&lt;/P&gt;&lt;P&gt;Hope this helps&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 May 2022 17:48:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1466384#M15732</guid>
      <dc:creator>MateoSegura413</dc:creator>
      <dc:date>2022-05-30T17:48:58Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS stuck in prvPortStartFirstTask</title>
      <link>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1586034#M20152</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have the same issue on the same example and I have FreeRTOS for S32K3 2.0.1.&lt;/P&gt;&lt;P&gt;Can someone explain what is the root cause of this?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Lucian&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jan 2023 13:06:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FreeRTOS-stuck-in-prvPortStartFirstTask/m-p/1586034#M20152</guid>
      <dc:creator>lucianmocanu_zzzzz</dc:creator>
      <dc:date>2023-01-20T13:06:18Z</dc:date>
    </item>
  </channel>
</rss>