<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic in which case should I use function ConfigTxMb? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1583208#M20032</link>
    <description>&lt;P&gt;I can send data only with the flexcan_drv_send function,&amp;nbsp;in which case should I use the function ConfigTxMb? This two func gets the same parameters.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In FLEXCAN_Set_TxMsgBuff, "Then this function will copy the user's buffer into the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;message buffer data area and configure the message buffer as required for&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;transmission."&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Why we need to "transmit message buffer configuration" ?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 17 Jan 2023 07:10:39 GMT</pubDate>
    <dc:creator>buccno</dc:creator>
    <dc:date>2023-01-17T07:10:39Z</dc:date>
    <item>
      <title>in which case should I use function ConfigTxMb?</title>
      <link>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1583208#M20032</link>
      <description>&lt;P&gt;I can send data only with the flexcan_drv_send function,&amp;nbsp;in which case should I use the function ConfigTxMb? This two func gets the same parameters.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In FLEXCAN_Set_TxMsgBuff, "Then this function will copy the user's buffer into the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;message buffer data area and configure the message buffer as required for&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;transmission."&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Why we need to "transmit message buffer configuration" ?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 07:10:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1583208#M20032</guid>
      <dc:creator>buccno</dc:creator>
      <dc:date>2023-01-17T07:10:39Z</dc:date>
    </item>
    <item>
      <title>Re: in which case should I use function ConfigTxMb?</title>
      <link>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1583398#M20037</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209588"&gt;@buccno&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please specify which MCU and software you are using?&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jan 2023 18:14:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1583398#M20037</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-01-16T18:14:47Z</dc:date>
    </item>
    <item>
      <title>Re: in which case should I use function ConfigTxMb?</title>
      <link>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1583709#M20049</link>
      <description>Ah sorry s32k116</description>
      <pubDate>Tue, 17 Jan 2023 06:49:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1583709#M20049</guid>
      <dc:creator>buccno</dc:creator>
      <dc:date>2023-01-17T06:49:54Z</dc:date>
    </item>
    <item>
      <title>Re: in which case should I use function ConfigTxMb?</title>
      <link>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1584199#M20076</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209588"&gt;@buccno&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The flexcan_driver.c file comes with a detailed explanation of the functions:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VaneB_0-1673992761537.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/207678i2E014F27FB29F3A9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VaneB_0-1673992761537.png" alt="VaneB_0-1673992761537.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VaneB_1-1673992793205.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/207679i8D9210BC13468C4A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VaneB_1-1673992793205.png" alt="VaneB_1-1673992793205.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Let me know if this does not clarify your inquiry.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 22:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1584199#M20076</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-01-17T22:02:01Z</dc:date>
    </item>
    <item>
      <title>Re: in which case should I use function ConfigTxMb?</title>
      <link>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1584433#M20085</link>
      <description>Actually, my confusion is, with configTxMb, we activated MB, cleared the corresponding IRQ flag, write the ID register in MB, write payload data bytes in MB, and updated the control and status word. But not need this configuration, I send data only using the flexcan_drv_send function.&lt;BR /&gt;&lt;BR /&gt;What's the benefit of flexcan_drv_configTxMb before sending data using? Which case should I use?</description>
      <pubDate>Wed, 18 Jan 2023 08:04:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1584433#M20085</guid>
      <dc:creator>buccno</dc:creator>
      <dc:date>2023-01-18T08:04:05Z</dc:date>
    </item>
    <item>
      <title>Re: in which case should I use function ConfigTxMb?</title>
      <link>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1585696#M20140</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209588"&gt;@buccno&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Using FLEXCAN_DRV_ConfigTxMb (configure TX message buffer with index TX_MSG_ID and TX_MAILBOX) before FLEXCAN_DRV_Send (execute send non-blocking), you ensure that the Mb is correctly configured to be used it.&lt;/P&gt;
&lt;P&gt;The usage of these functions together depends on your application, but one suggested case is to send data via CAN to the specified mailbox with the specified message-id.&lt;/P&gt;
&lt;P&gt;I hope this will help you&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jan 2023 19:25:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/in-which-case-should-I-use-function-ConfigTxMb/m-p/1585696#M20140</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-01-19T19:25:21Z</dc:date>
    </item>
  </channel>
</rss>