<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can not open the example from SDK in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Can-not-open-the-example-from-SDK/m-p/1578907#M19893</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;When I want to open a example project from SDK, I can open it successfully by S32DS,however, I can not open the ".mex" file.It shows that the pins tool was forbidden.&lt;/P&gt;&lt;P&gt;Then, I open the pins tool,but there is no pins that is configured in advance. Also, there is something wrong with the peripheral tools.It just shows that It can not find the drivers in toolchains or IDE and the project can not be compiled.&lt;/P&gt;</description>
    <pubDate>Mon, 09 Jan 2023 02:14:37 GMT</pubDate>
    <dc:creator>Hermit</dc:creator>
    <dc:date>2023-01-09T02:14:37Z</dc:date>
    <item>
      <title>Can not open the example from SDK</title>
      <link>https://community.nxp.com/t5/S32K/Can-not-open-the-example-from-SDK/m-p/1578907#M19893</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;When I want to open a example project from SDK, I can open it successfully by S32DS,however, I can not open the ".mex" file.It shows that the pins tool was forbidden.&lt;/P&gt;&lt;P&gt;Then, I open the pins tool,but there is no pins that is configured in advance. Also, there is something wrong with the peripheral tools.It just shows that It can not find the drivers in toolchains or IDE and the project can not be compiled.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Jan 2023 02:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-not-open-the-example-from-SDK/m-p/1578907#M19893</guid>
      <dc:creator>Hermit</dc:creator>
      <dc:date>2023-01-09T02:14:37Z</dc:date>
    </item>
    <item>
      <title>Re: Can not open the example from SDK</title>
      <link>https://community.nxp.com/t5/S32K/Can-not-open-the-example-from-SDK/m-p/1578947#M19895</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Hermit" target="_blank"&gt;Hi@Hermit&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;please click the &lt;STRONG&gt;Update Code&lt;/STRONG&gt; button then you can build the demo successfully!&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_1-1673235983207.png" style="width: 534px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/206416iCAE3FBED2F41819B/image-dimensions/534x247?v=v2" width="534" height="247" role="button" title="Senlent_1-1673235983207.png" alt="Senlent_1-1673235983207.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;This demo set the FlexCAN to Loop-Back mode, so it doesn't enable pins tool.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Jan 2023 03:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-not-open-the-example-from-SDK/m-p/1578947#M19895</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-01-09T03:46:57Z</dc:date>
    </item>
    <item>
      <title>Re: Can not open the example from SDK</title>
      <link>https://community.nxp.com/t5/S32K/Can-not-open-the-example-from-SDK/m-p/1578993#M19900</link>
      <description>&lt;P&gt;Hi Senlent,&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Jan 2023 05:48:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-not-open-the-example-from-SDK/m-p/1578993#M19900</guid>
      <dc:creator>Hermit</dc:creator>
      <dc:date>2023-01-09T05:48:33Z</dc:date>
    </item>
  </channel>
</rss>