<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Some problem in the process of debugging in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Some-problem-in-the-process-of-debugging/m-p/1577095#M19810</link>
    <description>&lt;P&gt;Hello Team,&lt;/P&gt;&lt;P&gt;I have some trouble in debugging. When I try to import the project from others, and I have built it successfully.After configuring, I try to debug. But there is something wrong with it.It just shows that it can not find the source file "main.c" at specific path.And the path might be others, not mine.Therefore, I can not debug it.The screenshot is attached.&lt;/P&gt;&lt;P&gt;What should I do to configure it? I need your help. Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best wishes,&lt;/P&gt;&lt;P&gt;Hermit.&lt;/P&gt;</description>
    <pubDate>Wed, 04 Jan 2023 11:57:18 GMT</pubDate>
    <dc:creator>Hermit</dc:creator>
    <dc:date>2023-01-04T11:57:18Z</dc:date>
    <item>
      <title>Some problem in the process of debugging</title>
      <link>https://community.nxp.com/t5/S32K/Some-problem-in-the-process-of-debugging/m-p/1577095#M19810</link>
      <description>&lt;P&gt;Hello Team,&lt;/P&gt;&lt;P&gt;I have some trouble in debugging. When I try to import the project from others, and I have built it successfully.After configuring, I try to debug. But there is something wrong with it.It just shows that it can not find the source file "main.c" at specific path.And the path might be others, not mine.Therefore, I can not debug it.The screenshot is attached.&lt;/P&gt;&lt;P&gt;What should I do to configure it? I need your help. Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best wishes,&lt;/P&gt;&lt;P&gt;Hermit.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jan 2023 11:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Some-problem-in-the-process-of-debugging/m-p/1577095#M19810</guid>
      <dc:creator>Hermit</dc:creator>
      <dc:date>2023-01-04T11:57:18Z</dc:date>
    </item>
    <item>
      <title>Re: Some problem in the process of debugging</title>
      <link>https://community.nxp.com/t5/S32K/Some-problem-in-the-process-of-debugging/m-p/1577554#M19817</link>
      <description>&lt;P&gt;Hi@&lt;U&gt;Hermit&lt;/U&gt;&lt;/P&gt;
&lt;P&gt;please check your project included path, some invaild paths may causes such errors!&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1672883537404.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/206131iA7CDBFFCE3C28A08/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Senlent_0-1672883537404.png" alt="Senlent_0-1672883537404.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_0-1672883537404.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 01:55:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Some-problem-in-the-process-of-debugging/m-p/1577554#M19817</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-01-05T01:55:35Z</dc:date>
    </item>
    <item>
      <title>Re: Some problem in the process of debugging</title>
      <link>https://community.nxp.com/t5/S32K/Some-problem-in-the-process-of-debugging/m-p/1577574#M19818</link>
      <description>&lt;P&gt;OK,thanks&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 02:19:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Some-problem-in-the-process-of-debugging/m-p/1577574#M19818</guid>
      <dc:creator>Hermit</dc:creator>
      <dc:date>2023-01-05T02:19:33Z</dc:date>
    </item>
  </channel>
</rss>