<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K LPSPI CIRFIFO Example in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-LPSPI-CIRFIFO-Example/m-p/1576406#M19774</link>
    <description>&lt;P&gt;Hi on the S32K344 For an SPI SD Card I would like to the use to MATCFG (Match0) and CIRFIFO functionality to get an interrupt when the SD card gets out of the busy state which means that DO gets high (0xFF).&lt;/P&gt;
&lt;P&gt;It seems that the S32K3 LPSPI RTD doesn't implement the CIRFIFO functionality is there are example available on how to enter CIRFIFO to send repeated data (0xFF) and wait until DO matches (0xFF) using MATCFG and an interrupt and then exit CIRFIFO cleanly?&lt;/P&gt;</description>
    <pubDate>Tue, 03 Jan 2023 07:57:59 GMT</pubDate>
    <dc:creator>petervdperk</dc:creator>
    <dc:date>2023-01-03T07:57:59Z</dc:date>
    <item>
      <title>S32K LPSPI CIRFIFO Example</title>
      <link>https://community.nxp.com/t5/S32K/S32K-LPSPI-CIRFIFO-Example/m-p/1576406#M19774</link>
      <description>&lt;P&gt;Hi on the S32K344 For an SPI SD Card I would like to the use to MATCFG (Match0) and CIRFIFO functionality to get an interrupt when the SD card gets out of the busy state which means that DO gets high (0xFF).&lt;/P&gt;
&lt;P&gt;It seems that the S32K3 LPSPI RTD doesn't implement the CIRFIFO functionality is there are example available on how to enter CIRFIFO to send repeated data (0xFF) and wait until DO matches (0xFF) using MATCFG and an interrupt and then exit CIRFIFO cleanly?&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jan 2023 07:57:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-LPSPI-CIRFIFO-Example/m-p/1576406#M19774</guid>
      <dc:creator>petervdperk</dc:creator>
      <dc:date>2023-01-03T07:57:59Z</dc:date>
    </item>
  </channel>
</rss>