<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックProblem with receving using UART in s32k144  board</title>
    <link>https://community.nxp.com/t5/S32K/Problem-with-receving-using-UART-in-s32k144-board/m-p/1575493#M19701</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Iam working on a project where I need to use UART for communication. while I tried the examples of the UART Iam able to transmit the data but not able to receive the data.&amp;nbsp;&lt;/P&gt;&lt;P&gt;While debugging I got to know that receive status is always busy.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ramsai_0-1672303379654.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205685i6323C16C29C98AF6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ramsai_0-1672303379654.png" alt="Ramsai_0-1672303379654.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any suggestion to clear the issue?&lt;/P&gt;&lt;P&gt;MCU-S32K144&lt;/P&gt;&lt;P&gt;IDE-S32KDS 2.2V&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ram&lt;/P&gt;</description>
    <pubDate>Thu, 29 Dec 2022 08:45:25 GMT</pubDate>
    <dc:creator>Ramsai</dc:creator>
    <dc:date>2022-12-29T08:45:25Z</dc:date>
    <item>
      <title>Problem with receving using UART in s32k144  board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-with-receving-using-UART-in-s32k144-board/m-p/1575493#M19701</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Iam working on a project where I need to use UART for communication. while I tried the examples of the UART Iam able to transmit the data but not able to receive the data.&amp;nbsp;&lt;/P&gt;&lt;P&gt;While debugging I got to know that receive status is always busy.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ramsai_0-1672303379654.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205685i6323C16C29C98AF6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ramsai_0-1672303379654.png" alt="Ramsai_0-1672303379654.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any suggestion to clear the issue?&lt;/P&gt;&lt;P&gt;MCU-S32K144&lt;/P&gt;&lt;P&gt;IDE-S32KDS 2.2V&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ram&lt;/P&gt;</description>
      <pubDate>Thu, 29 Dec 2022 08:45:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-with-receving-using-UART-in-s32k144-board/m-p/1575493#M19701</guid>
      <dc:creator>Ramsai</dc:creator>
      <dc:date>2022-12-29T08:45:25Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with receving using UART in s32k144  board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-with-receving-using-UART-in-s32k144-board/m-p/1576014#M19739</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;if you refer to demo example (pluart_echo) it is written in the way the received chars are stored into user buffer and the reception stops when newline character (\n) is received or the buffer is full, then received data are echoed back. You can check if buffer is filled within debugger.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jan 2023 09:37:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-with-receving-using-UART-in-s32k144-board/m-p/1576014#M19739</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-01-02T09:37:36Z</dc:date>
    </item>
  </channel>
</rss>