<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to receive Standard Message ID in CAN-FD ? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/How-to-receive-Standard-Message-ID-in-CAN-FD/m-p/1570419#M19454</link>
    <description>&lt;P&gt;Pls review my test project attached file is same as real project and the result also same.&lt;/P&gt;&lt;P&gt;As your advise I did MIXED setting.&lt;/P&gt;&lt;P&gt;In attached file you find test code in main.c.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 15 Dec 2022 11:24:41 GMT</pubDate>
    <dc:creator>dnewbe</dc:creator>
    <dc:date>2022-12-15T11:24:41Z</dc:date>
    <item>
      <title>How to receive Standard Message ID in CAN-FD ?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-receive-Standard-Message-ID-in-CAN-FD/m-p/1568973#M19411</link>
      <description>&lt;P&gt;Hi dear all CAN expert&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My code run and receive Extended Message ID in CAN-FD mode. My board have S32K312 MCU.&lt;/P&gt;&lt;P&gt;But I didn't receive Standard Message ID.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did config CAN-FD configuration on MCAL driver (PlatformSDK_S32K3_2207).&lt;/P&gt;&lt;P&gt;The configuration are&lt;/P&gt;&lt;P&gt;Can Rx/Tx Processing Type is POLLING&lt;/P&gt;&lt;P&gt;CanBaudrateTypeSuport is NORAM_CBT&lt;/P&gt;&lt;P&gt;Can Controller BaudRate 500 Kbps and Can FD Controller BaudRate 2 Mbps&lt;/P&gt;&lt;P&gt;CanRxFiFo is CanEnhanceFiFo&lt;/P&gt;&lt;P&gt;CanEnhanceFiFo is MASK_FILTER_SCHEME&lt;/P&gt;&lt;P&gt;Can Type is BASIC&lt;/P&gt;&lt;P&gt;Can ID Message Type is EXTENDED&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And test code is&lt;/P&gt;&lt;P&gt;rx_info.msg_id_type = FLEXCAN_MSG_ID_EXT;&lt;BR /&gt;FlexCAN_Ip_ConfigRxMb(CanController_0, 1, &amp;amp;rx_info, 0x1000);&lt;/P&gt;&lt;P&gt;rx_info.msg_id_type = FLEXCAN_MSG_ID_STD;&lt;BR /&gt;FlexCAN_Ip_ConfigRxMb(CanController_0, 2, &amp;amp;rx_info, 0x20);&lt;/P&gt;&lt;P&gt;rx_info.msg_id_type = FLEXCAN_MSG_ID_EXT;&lt;BR /&gt;FlexCAN_Ip_ConfigRxMb(CanController_0, 3, &amp;amp;rx_info, 0x3000);&lt;/P&gt;&lt;P&gt;rx_info.msg_id_type = FLEXCAN_MSG_ID_STD;&lt;BR /&gt;FlexCAN_Ip_ConfigRxMb(CanController_0, 4, &amp;amp;rx_info, 0x40);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I receive is only Extended Message.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't know how to config also to receive Standard Message ID type.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Dec 2022 11:54:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-receive-Standard-Message-ID-in-CAN-FD/m-p/1568973#M19411</guid>
      <dc:creator>dnewbe</dc:creator>
      <dc:date>2022-12-13T11:54:59Z</dc:date>
    </item>
    <item>
      <title>Re: How to receive Standard Message ID in CAN-FD ?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-receive-Standard-Message-ID-in-CAN-FD/m-p/1569203#M19419</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202910"&gt;@dnewbe&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do you already test defining the&amp;nbsp;&lt;SPAN&gt;Can ID Message Type as MIXED?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VaneB_2-1670971049004.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/204276iE632BC800771E88A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VaneB_2-1670971049004.png" alt="VaneB_2-1670971049004.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;B.R.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;VaneB&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Dec 2022 22:37:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-receive-Standard-Message-ID-in-CAN-FD/m-p/1569203#M19419</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2022-12-13T22:37:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to receive Standard Message ID in CAN-FD ?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-receive-Standard-Message-ID-in-CAN-FD/m-p/1569283#M19420</link>
      <description>&lt;P&gt;Yes I did test with MIXED but the result is same.&lt;/P&gt;&lt;P&gt;Also I did another configuration STANDARD but configuration too complicate to understand so I can't complete configuration.&lt;/P&gt;&lt;P&gt;At this time I continue trying...&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 01:58:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-receive-Standard-Message-ID-in-CAN-FD/m-p/1569283#M19420</guid>
      <dc:creator>dnewbe</dc:creator>
      <dc:date>2022-12-14T01:58:27Z</dc:date>
    </item>
    <item>
      <title>Re: How to receive Standard Message ID in CAN-FD ?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-receive-Standard-Message-ID-in-CAN-FD/m-p/1569955#M19442</link>
      <description>&lt;P&gt;Given the use case you are trying to implement, it seems that MIXED is the configuration you need.&lt;/P&gt;
&lt;P&gt;At this moment, you are using EXTENDED configuration, which does not support standard CAN messages, that could be why you are not receiving these specific standard frames.&lt;/P&gt;
&lt;P&gt;MIXED should allow you to receive both standard and extended CAN frames. Just as a note, even though the configuration is MIXED, "standard and RECEIVE type will be treated as EXTENDED", as shown in config tools.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 20:01:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-receive-Standard-Message-ID-in-CAN-FD/m-p/1569955#M19442</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2022-12-14T20:01:42Z</dc:date>
    </item>
    <item>
      <title>Re: How to receive Standard Message ID in CAN-FD ?</title>
      <link>https://community.nxp.com/t5/S32K/How-to-receive-Standard-Message-ID-in-CAN-FD/m-p/1570419#M19454</link>
      <description>&lt;P&gt;Pls review my test project attached file is same as real project and the result also same.&lt;/P&gt;&lt;P&gt;As your advise I did MIXED setting.&lt;/P&gt;&lt;P&gt;In attached file you find test code in main.c.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 11:24:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-receive-Standard-Message-ID-in-CAN-FD/m-p/1570419#M19454</guid>
      <dc:creator>dnewbe</dc:creator>
      <dc:date>2022-12-15T11:24:41Z</dc:date>
    </item>
  </channel>
</rss>